RT1050 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 SDK

927 Views
krischeng
Contributor I

RT1050使用的SDK是哪一版的,我目前從網路上下載的版本是2.3.0,但似乎沒有LCDsample code

Labels (1)
0 Kudos
Reply
1 Reply

863 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

非常感谢使用NXP产品,很高兴为你提供技术支持!

请到官网下载,现在版本已到2.7.0,里面有LCD显示的例程,还有与emWin,LittlevGL图像软接库相结合的例程。

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply