RT1050 FlexSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 FlexSPI

3,534件の閲覧回数
christiangradl
Contributor III

Hi,

i want to connect my RT1050 to a FPGA via FlexSPI, using Hyberbus.

The max. clock freq is limited to 166 MHz.

Please can you tell me if these calculation is correct:

spi clock freq. 166 MHz => 332 MByte/sec (8 Bit Hyperbus) => DDR mode

The command and address settings takes about 13 Cycles, but the i can read with 332 MByte/sec.

Is this correct?

Thanx

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,301件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Christian,

2 points:

- Can you please clarify and provide more details on how are you doing this calculations?

- FPGA device should be accessed by AHB command. All AHB accesses to FPGA will be transparent to SW driver (no SW intervention).There may be some special requirements from FPGA device. You can find this information on chapter 30.8.6 Application on FPGA device in the IMXRT1050 Reference Manual


Regards,
Carlos
NXP Technical Support

0 件の賞賛
返信

2,301件の閲覧回数
christiangradl
Contributor III

Hi Carlos

There are 3 connection lines between i.mx and FPGA:

QSPI (332 MHz, Hyperbus)

1 SPI (30 MHz, LPSPI)

EMC 16 bit Databus (100 MHz, SEMC, Reference Manual 49.4.9)

What do you mean with “FPGA device should be accessed by AHB command”

As mentioned in the Reference Manual 49.4.9, I can configure the SEMC for external SRAM access.

I set all waitstates, etc, to 0, then I setup the CS to 0x90000000 and then I can read/write through SEMC.

Do you think that this will not work?

Christian

Von: Carlos_Musich

Gesendet: Dienstag, 15. Mai 2018 23:27

An: Christian Gradl <christian.gradl@sigmatek.at>

Betreff: Re: - Re: RT1050 FlexSPI

NXP Community <https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Cchristian.gradl%40sigmatek.at%7Cd98d57c9024c49833c2408d5baaaa387%7Cbcb1d87ad2bc486ea62b9ac9c746bc1b%7C0%7C0%7C636620164426034670&sdata=VCipZDGu%2BrFJqT%2FnNx5dDnHR%2FrvraiH6eBYVHLKuh5E%3D&reserved=0>

Re: RT1050 FlexSPI

reply from Carlos_Musich<https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2FCarlos_Musich%3Fet%3Dwatches.email.thread&data=02%7C01%7Cchristian.gradl%40sigmatek.at%7Cd98d57c9024c49833c2408d5baaaa387%7Cbcb1d87ad2bc486ea62b9ac9c746bc1b%7C0%7C0%7C636620164426034670&sdata=UBmyWgD%2FDOVmsydtEaWn2xQEQxPTfjLX65hcUni8gEk%3D&reserved=0> in i.MX Community - View the full discussion<https://emea01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1014754%3FcommentID%3D1014754%26et%3Dwatches.email.thread%23comment-1014754&data=02%7C01%7Cchristian.gradl%40sigmatek.at%7Cd98d57c9024c49833c2408d5baaaa387%7Cbcb1d87ad2bc486ea62b9ac9c746bc1b%7C0%7C0%7C636620164426034670&sdata=19ONt6E4g2jqBgICUhejVySsh9H2DaPmooX0UXYZQ6M%3D&reserved=0>

0 件の賞賛
返信