Hello,
I have been trying to make my RT1050-EVK (REV A) boot from SD card, by following the instructions in AN12107.pdf. All the steps up to and including the MfgTool flashing process complete successfully, however when I re-configure the board for execution (SW7: 1010, J1:5-6, USB:J28), nothing appears on the terminal.
I have adjusted the MIMXRT1052xxxxx_ram.icf IAR linker file as per the instructions (m_interrupts_start @ 0x00002000, m_text_start @ 0x00002400). The SD card used in J20 is a brand-new 16 GB SanDisk Ultra HC I; when I manually zero the card device, and then flash it with MfgTool and examine it, I am able to see some data on it, starting at 0x400 as expected.
When I follow the steps for XIP'ing form Hyperflash, or even from QSPI as per AN12108.pdf (on a different board with Hyperflash removed), everything works perfectly. I am using version 1.1 of the Flashloader tools.
Could you please advise on how to resolve the issue?
Thanks in advance,
Nikos
解決済! 解決策の投稿を見る。
Hello,
You may try modifying the StartAddress in "imx-itcm-unsigned.bd" file to below
0x2000. I used startAddress = 0x1000 instead of 0x8000 in "imx-itcm-unsigned.bd".
It works on my board!
Regards,
Yuri.
You can try this GUI tool, it supports eMMC
Hello,
You may try modifying the StartAddress in "imx-itcm-unsigned.bd" file to below
0x2000. I used startAddress = 0x1000 instead of 0x8000 in "imx-itcm-unsigned.bd".
It works on my board!
Regards,
Yuri.
Thanks Yuri, that was spot-on! After changing startAddress to 0x1000 in "imx-itcm-unsigned.bd", I can now boot from SD to ITCM.