RT1050 ENET_INT pin direction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 ENET_INT pin direction

Jump to solution
1,351 Views
felix1
Contributor IV

Hi,

according to RT1050 EVK, pin ENET_INT pin is input, 

felix1_0-1702452481698.png

In SDK example evkbimxrt1050_lwip_ping_freertos and other lwip examples,

the ENET_INT (GPIO_AD_B0_10) seems output, do I miss something?

int main(void)
{
    gpio_pin_config_t gpio_config = {kGPIO_DigitalOutput, 0, kGPIO_NoIntmode};

    BOARD_ConfigMPU();
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitDebugConsole();
    BOARD_InitModuleClock();

    IOMUXC_EnableMode(IOMUXC_GPR, kIOMUXC_GPR_ENET1TxClkOutputDir, true);

    GPIO_PinInit(GPIO1, 9, &gpio_config);
    GPIO_PinInit(GPIO1, 10, &gpio_config);
    /* Pull up the ENET_INT before RESET. */
    GPIO_WritePinOutput(GPIO1, 10, 1);
    GPIO_WritePinOutput(GPIO1, 9, 0);
    SDK_DelayAtLeastUs(10000, CLOCK_GetFreq(kCLOCK_CpuClk));
    GPIO_WritePinOutput(GPIO1, 9, 1);

 

0 Kudos
Reply
1 Solution
1,285 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry it should be as input, how is mentioned in the RM.

Best regards,
Pavel

View solution in original post

0 Kudos
Reply
9 Replies
1,339 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I will review it, and in case the error reporting is right, I will need the information on the version of the schematic. Could you share more information about where you see this?

Best regards,
Pavel 

0 Kudos
Reply
1,322 Views
felix1
Contributor IV

Hi  Pavel,

You can see the schematic in the attached file.

In the reference manual, it also set as input, so I doubt the example do this operation for some purpose.

felix1_0-1702519348173.png

 

 

0 Kudos
Reply
1,310 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I made the report, and the team confirmed the issue was reported before, they will update this in the next release.

Best regards,
Pavel

0 Kudos
Reply
1,305 Views
felix1
Contributor IV
Hi Pavel,
Can you tell me ENET_INT should be input or output first? I need this information to correct my code.
0 Kudos
Reply
1,286 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry it should be as input, how is mentioned in the RM.

Best regards,
Pavel

0 Kudos
Reply
1,204 Views
felix1
Contributor IV

Hi Pavel,

1) In example evkbimxrt1050_lwip_ping_freertos, except to change ENET_INT as input, what else should I do?

2) Where can I find example evkbimxrt1050_lwip_ping_freertos in the mcuxpresso github 

https://github.com/nxp-mcuxpresso/mcux-sdk/tree/main/boards/evkbimxrt1050 ?

0 Kudos
Reply
1,179 Views
MultipleMonomials
Contributor III

Wait, hold up, I've run into this issue before in my testing. ENET_INT actually is an output pin, in a way.  The reason is, the ENET_INT pin actually does double duty as the NAND_TREE strapping pin on the PHY

MultipleMonomials_0-1703030488622.png

This means that when reset is released for the phy, the ENET_INT line needs to be logic high so that the phy doesn't go into NAND_TREE test mode (which makes it basically inert).

If you wish to use the ENET_INT line to get interrupts from the phy, you can use it as an input, you just have to reconfigure it to input after the phy has been reset and has booted up. 

However, you may run into issues because of an error in the schematic that I noticed: the ENET_INT line is both pulled up and pulled down by resistors!

MultipleMonomials_1-1703030854416.png

MultipleMonomials_2-1703030868468.png

This means it will quite possibly be stuck at 1.6V unless you remove the pulldown resistor from your eval kit. This screenshot is from the 1060 EVK rev B, unsure if other EVKs have the same issue.

0 Kudos
Reply
1,140 Views
felix1
Contributor IV

Hi @MultipleMonomials ,

Thanks for your information.

My customer board solder both the pull-up and pull-down resistors for ENET_INT pin as EVK, so it output 1.65V to PHY. 

According to your test, any problem you meet?

0 Kudos
Reply
949 Views
MultipleMonomials
Contributor III

It seems like, on the EVK board, we do get away with it and the phy recognizes it as a logic high.  But I'm not sure I'd trust that on a production board.

0 Kudos
Reply