RT1050 Crystal Spec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 Crystal Spec

1,453 Views
martinsmith
Contributor III

Hi, I'm looking for an exact spec for the xtal on the RT1050. The datasheet gives a bit of a incomplete spec. Would the crystals mentioned in this thread do the job? https://community.nxp.com/thread/308944  

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,223 Views
martinsmith
Contributor III

Thanks Igor, I have selected the FA-20H 24.0000MF20X-K3 from Epson which I think meets all the requirements.

0 Kudos
Reply

1,223 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

since i.MX and Vybrid parts use many same IP modules and particular XTALOSC,

crystals mentioned on that thread also can be used with RT1050. Seems most full

characteristics are given in Table 9. Recommended External Crystal Specifications

i.MX25 Datasheet

https://www.nxp.com/docs/en/data-sheet/IMX25CEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply