RT1024 USB Audio 2.0 Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1024 USB Audio 2.0 Windows 10

1,080 Views
asarbs
Contributor II

I;m working on some product that is using USB Audio 2.0. I have a communication from Linux Machines to my device via USB Audio 2.0 with out any problems, the same code on Windows 10 don't work, in Device Manager I got information about error code 10 "The specified range cannot be found in the range list" In Details under "problem status" i have 0xc000028c witch indicates that this might be an issue with Windows Driver? I'm attaching dump from USBView tool from Windows Debug toolkit with my USB descriptors configuration. 

Any advice? 

Labels (1)
0 Kudos
Reply
5 Replies

1,028 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @asarbs,

Could you please try enabling the "USB_DEVICE_WORKAROUND_AUDIO_20_WINDOWS" macro definition under "usb_device_descriptor.h" file and let me know if this solves the issue?

BR,
Edwin.

0 Kudos
Reply

983 Views
asarbs
Contributor II

Hi,

Sorry for late response, I have missed notification mail. 

 

Unfortunately in my  code base I don't have any "USB_DEVICE_WORKAROUND_AUDIO_20_WINDOWS" macro. 

0 Kudos
Reply

974 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @asarbs,

I would highly suggest you base your USB audio 2.0 application on our SDK drivers and examples, so you can enable the "USB_DEVICE_WORKAROUND_AUDIO_20_WINDOWS" macro that provides a workaround for the issue between the USB stack and Windows machines.

BR,
Edwin.

0 Kudos
Reply

959 Views
asarbs
Contributor II

I have based my solution on Examples and MCUXpresso IDE tool. We are glued to  SDK v2.13.0 Was USB_DEVICE_WORKAROUND_AUDIO_20_WINDOWS implemented in higher version? 

0 Kudos
Reply

945 Views
asarbs
Contributor II

OK, I see that USB_DEVICE_WORKAROUND_AUDIO_20_WINDOWS is available in SDK 2.16. Thanks for your support.  

Tags (1)
0 Kudos
Reply