RT1021 FlexSPI IPCMDDONE interrupt/flag appears to arrive early when reading?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 FlexSPI IPCMDDONE interrupt/flag appears to arrive early when reading?

755 Views
rshipman
Contributor V

Hi,

I am using the fsl_flexspi.c driver to access NOR flash. The blocking API seems to work ok, but when I switched to the non-blocking functions, I found that reading from flash failed for a 4096 block. In fact, it fails for any block length > 8 bytes.

If I read a block of 4096 bytes, the IPCMDDONE flag is raised before all the bytes are received. It seems to consistently occur when 120 bytes are remaining to be read. If I modify the isr so that it effectively ignores the IPCMDDONE flag, then it carries on receiving bytes and I get the full 4096 byte block. So I have modified fsl_flexspi.c to workaround this issue.

My questions are:

  • Is this expected behaviour? Shouldn't the IPCMDDONE flag be raised when all 4096 bytes have arrived?
  • Is there something missing from the driver? E.g. another flag to check?
  • Am I simply not setting something correctly?

I have uploaded my demo project that shows this problem.

It is basically the evkmimxrt1020_iled_blinky demo with evkmimxrt1020_flexspi_nor_polling_transfer merged in. The demo is modified so that it runs from internal ram (SRAM_OC). I have copied the file flexspi_nor_flash_ops.c to flexspi_nor_flash_ops_non_blocking.c. Both files have been modified, the latter uses the non-blocking api.

Note:

  • Both I and D caches are disabled.
  • I'm not using the AHB feature - disabled.

In main() it does the following (after the initialisation etc):

  • Blocking: erase chip.
  • Blocking: program 4096 bytes using a repeating pattern of 1 - 0x80.
  • Blocking: readback and check it is correct.
  • Non-blocking: readback and check it is correct. This fails without my workaround.
  • Non-blocking: erase chip
  • Non-blocking: readback and check. This fails without my workaround.
  • Non-blocking: program 4096 bytes using a repeating pattern of 1 - 0x80.
  • Non-blocking: readback and check. This fails without my workaround.
  • Non-blocking: erase sector
  • Non-blocking: readback and check. This fails without my workaround.
  • Flash led when done.

In MCUXpresso change the settings so that the preprocessor symbol is as follows:

  • To see the problem.
    • EARLY_IPCMDDONE_WORKAROUND=0
  • To enable the workaround
    • EARLY_IPCMDDONE_WORKAROUND=1

This is what I saw with different block lengths (change TEST_BLOCK_SIZE):

Block length bytesRemainder when IPCMDDONE receivedResult
4096120Fail
2048120Fail
1024120Fail
512120Fail
256120Fail
128112Fail
6448Fail
3224Fail
168Fail
80Pass
40Pass
10Pass

 

The workaround is as follows (not necessarily the best way):

  • In the FlexSPI ISR in fsl_flexspi.c (FLEXSPI_TransferHandleIRQ):
    • When the IPCMDDONE interrupt flag appears:
      • If we are expecting more data, then we just make a note that the IPCMDDONE interrupt has been received.
      • If all the data has been received, then we call the callback.
    • When the number of bytes we are expecting has been received then
      • If IPCMDDONE interrupt flag has been seen, then we call the callback.
      • If IPCMDDONE interrupt flag has not been seen, then we wait for it.

IMPORTANT: This mechanism relies on the flexspi_transfer_t::dataSize field being set to a valid size or zero for this to work, especially for commands that do not take a size, such as chip erase. If dataSize is set to a non-zero value for chip erase etc, then the callback will not be called.


Info:

  • MCUXpresso v11.9.1
  • SDK_2_15_100_EVK-MIMXRT1020
  • Eval board: MIMXRT1020-EVK, SCH-29856 REV A3, TDA6595, 700-29856 REV A, TR18290644
  • Our own prototype board exhibits this behaviour as well. (Based on RT1021, with a Micron flash fitted.)

Thanks for your help.

Kind regards.

Labels (1)
0 Kudos
Reply
1 Reply

716 Views
Habib_MS
NXP Employee
NXP Employee

Hello @rshipman ,

Thank you for providing us this workaround solving the problem, I'm going to contact the internal SDK group so they can deliberate about the addition of this fix on a future SDK release.

With respect of your questions, as soon as we have a correct answer to these, we will let you know.

 

BR,
Habib.

0 Kudos
Reply