RT1020 SDK: evkmimxrt1020_sdram_ini_dcd.c or evkmimxrt1020_sdram_ini_dcd.h missing?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1020 SDK: evkmimxrt1020_sdram_ini_dcd.c or evkmimxrt1020_sdram_ini_dcd.h missing?

846 次查看
klau
Contributor II

Hi,

I created a RT1020 SDK, more than once, from a button in the middle of this page labelled as "GET MCUXPRESSO SDK".
https://www.nxp.com/document/guide/get-started-with-the-mimxrt1020-evk:GS-MIMXRT1020-EVK

I believe that these files are needed to access SDRAM (external DRAM, not on chip RAM).
Am I correct?

If yes, could you show me how to get these two files please?
If these are missing from SDK, could you show me how to add them?

Thanks,
Kevin

0 项奖励
回复
2 回复数

826 次查看
klau
Contributor II

Hi,

Please refer to this post,
https://community.nxp.com/t5/i-MX-RT/How-to-generate-dcd-bin-file-for-mfgtools-use-to-flash-RT1020/m...

In the middle of that post, you will find 

"For an example, look at dcd_data[]

in “evkmimxrt1020_sdram_ini_dcd.c” of i.MX RT1020 SDK."

I could NOT find it in my SDK.

Could you help locate it please?

 

Thanks,
Kevin

0 项奖励
回复

808 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Kevin,

Please make sure you are selecting all the middleware when you build your SDK. Once you have done this you will find the files in the following path.

SDK_2.8.2_EVK-MIMXRT1020\middleware\safety_iec60730b\boards\evkmimxrt1020\xip

Regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复