RT1020/RT1050 ref manual issue?: BT_MPU_DISABLE and L1 I-Cache DISABLE fuses.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1020/RT1050 ref manual issue?: BT_MPU_DISABLE and L1 I-Cache DISABLE fuses.

965 Views
rshipman
Contributor V

Hi,

In the manual:

i.MX RT1020 Processor Reference Manual, Rev. 1, 12/2018

Table 21-9. Fusemap Descriptions

Page 1116

The table specifies:

0x470[1] BT_MPU_DISABLE

0x470[2] L1 I-Cache DISABLE

However in the tables:

Table 21-2. FlexSPI (Serial NOR) boot fusemap, page 1098

Table 21-3. SD boot fusemap, page 1100

Table 21-4. MMC/eMMC boot fusemap, page 1102

Table 21-5. SEMC (NAND) boot fusemap, page 1103

Table 21-6. SEMC (NOR) boot fusemap, page 1105

Table 21-7. FlexSPI1 (Serial NAND) boot fusemap, page 1106

The tables show:

0x470[1] L1 D-Cache DISABLE

0x470[2] L1 I-Cache DISABLE

So what does 0x470[1] actually do?

The same issue exists in the RT1050 Reference Manual as well, so if this is a mistake, it might be worth checking the RMs of all similar devices:

i.MX RT1050 Processor Reference Manual, Rev. 3, 8/2019

Kind regards,

Ronnie

Labels (2)
0 Kudos
Reply
1 Reply

890 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

0x470[1] L1 D-Cache DISABLE

0x470[2] L1 I-Cache DISABLE

Should be correct. Thanks for your feedback and we will forward it to the related team.

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply