Hi there,
I got a couple of questions about the schematic of the RT1020 Evaluation Kit. There are quite a few pins which are connected to multiple different periphals. I totally understand that this is a demo board and that it is supposed to support as many features as possible, but there are a few odd ones:
ENET-RST and JTAG-TDO
These two are both connected to pin AD_B0_04. Isn't that an issue for example during debugging with JTAG and using Ethernet at the same time?
On an own design it should be possible to use another pin for ENET_RST because it is software defined and not "directly" connected to the ethernet periphal, or am I wrong?
ENET and SPI on the Arduino Header
These seem to colide aswell on pins AD_B0_11 / 12 / 13 / 10. I think that's due to constraints being a demo board?
Thank you for your patience.
All the best