RT101x LPSPI API Master Blocking Transfer No SDI Signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT101x LPSPI API Master Blocking Transfer No SDI Signal

625件の閲覧回数
vishayp
Contributor I

On a custom RT1011 platform I am trying to bring up some SPI peripherals, but I see no signal on the SDI pin configured in the pin mux tool. I do see the SPI clock signal on the scope from its configured pin with the expected number of cycles as the number of bits I am writing.

I am using the LPSPI1 peripheral, SCK on GPIO_AD_06, SDI on GPIO_AD_03, SDO on GPIO_AD_04, CS not used, LPSPI API Master Blocking Transfer. What am I missing here?

ラベル(1)
0 件の賞賛
返信
1 返信

620件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
For the SPI master device, the SDI pin is a MISO pin of the SPI interface, it doesn't have signals otherwise, the slave device transfers the data to the master device.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信