RT101X USB FS/HS device without external crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT101X USB FS/HS device without external crystal

ソリューションへジャンプ
1,737件の閲覧回数
jh0
Contributor IV

Does RT101X can work as FS or / and HS USB device (not host) without using external crystal?

Regards,

JH

0 件の賞賛
返信
1 解決策
1,731件の閲覧回数
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals

元の投稿で解決策を見る

1 返信
1,732件の閲覧回数
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals