I now have the app note code built on the IAR tools it requires. Now I am trying to get the code into my RT1010 EVK, IAR tools complain that no J-Link debugger is found. Is a J-Link debug required to be used or is there a way of using the debug connction built into the RT1010 EVK with IAR tools.
Best Regards
Tom M.
Hello Tom,
The firmware of the on-board debugger on your EVK must me CMSIS instead of JLink and the project you are trying to run on IAR must be configured for a JLink debugger. To change this please follow the next steps:
That's it, now your application will stop looking for a JLink debugger.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------