QSPI Flash drivers RT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI Flash drivers RT1050

Jump to solution
1,148 Views
rubensjunior
Contributor IV

Dear friends,

We are developing a project to use the MIMXRT1051 processor and we intend to use one of the flash memories below, and for validation tests we ask your help because we do not have the drivers (.cfx), for QSPI flash, of these memories for the RT1050 processor.

Memories Partnumbers:

IS25LP128

IS25LP064A-JBLE

MT25QL512

W25N01GVZEIG


Thank you very much.

Rubens Júnior

1 Solution
954 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Unfortunately,We don't have the specific .cfx file for the part numbers you provided, you can try the IS25WP064A .cfx.Hope it help you. Have a nice day.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

1 Reply
955 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Unfortunately,We don't have the specific .cfx file for the part numbers you provided, you can try the IS25WP064A .cfx.Hope it help you. Have a nice day.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.