Hello , All
Customer (panasonic ) is using Jlink debugger to writing customer program(based on RT1060) into flash of RT106F board and wants to debug& boot the program.
The written process is ok , but the boot & debug fails
(I attached the jlink log and picture)
Panasonic uses flash and SDRAM in RT106F board as follows
QSPI-Flash:IS25LP512M-JLLE 512Mb,133MHz
SDRAM: IS42S16160J-6BLI 256Mb,166MHz
The sample project of Hello_world can be run on RAM in RT106F.
We tried to change the reset type and confirmed that
1 The boot mode is internal mode (2b10),
2 the DCD is using evkmimxrt1060_sdram_ini_dcd.c.
3. The macro definition of XIP_BOOT_HEADER_DCD_ENABLE is enabled
4.we set breaking point in ResetISR, the debug will not stop at Breaking point.
I wonder if we need to change the XIP file for the QSPI-Flash:IS25LP512M-JLLE ?
Could anyone give some advice?
@hiroshihiraga
@lucas_cao
@jay_heng
@chaosheng.xiang@nxp.com
@jorge_a_vazquez
Best regards
ZHOU