Production files for 1MW chip with IMX.RT 1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Production files for 1MW chip with IMX.RT 1064

665 Views
bshannon
Contributor III

My company has performed an evaluation of the Murata 1MW chip with NXP's IMXRT 1064 (no Linux OS). We are pleased with the results and are planning to use the 1MW in our design. From the SDK examples, I noticed that it reference various files to download to the 1MW (Bluetooth patch file, Wifi NVRAM). Once we go to production where should we get the most recent files, from Murata's GitHub or NXP's recent SDKs? Also are there any additional files that we need to download to the 1MW for production?

Tags (3)
0 Kudos
Reply
1 Reply

646 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

We do not have official support for 1MW with RT1064 SDK. Therefore, I would recommend to check and confirm with Murata for latest updates and most recent files.

Best regards,

Felipe

0 Kudos
Reply