Problem into debugging with CMSIS-DAP on IMXRT1050-EVKB board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem into debugging with CMSIS-DAP on IMXRT1050-EVKB board

2,486 次查看
GottiLuca
Contributor IV

I've just received a new IMXRT1050-EVKB board, but i cannot debug by CMSIS-DAP interface in MCUExpresso V10.2.1 .

I copied & pasted the consolle message :

"

MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 2018 11:25:37 - crt_emu_cm_redlink build 555)
Found chip XML file in C:/Users/LGotti/Documents/MCUXpressoIDE_10.2.1_795/workspace/evkbimxrt1050_hello_world/Debug\MIMXRT1052xxxxB.xml
Reconnected to existing link server
Connecting to probe 3 core 0:0 (using server started externally) gave 'OK'
Probe Firmware: CMSIS-DAP (ARM)
Serial Number: 0227000041114e45003a3009c207001692d1000097969900
VID:PID: 0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#9&2e1e48c8&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0:0 after searching for a good core
connection failed - Nn(05). Wire ACK Wait in DAP access.. Retrying
Using memory from core 0:0 after searching for a good core
Failed on connect: Nn(05). Wire ACK Wait in DAP access
Connected&Reset. Was: NotConnected. DpID: 00000000. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
Debug bus selected: MemAp 0
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
error closing down debug session - Nn(05). Wire ACK Wait in DAP access

"

Any hints to solve this problems ?

Thanks,

Luca

0 项奖励
回复
3 回复数

2,174 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Luca,

   It seems that you connected wrong connector.

  if you are using OpenSDA on board(DAP LINK), J28 should be connected to your PC usb port via usb otg cable.

Before debugging it, suggest you'd better read and understand schematic of i.MXRT1050 EVK,  which can help you do well in future design.

Check it, please!

Have a nice day!

Best Regards,

NXP TIC weidong sun

0 项奖励
回复

2,174 次查看
GottiLuca
Contributor IV

Dear Mr. Sun,

I have connected on J28 connector with the USB cable supplied with the board.

I've done the same on another new EVK ordered which I can debug without problem.

But the first pcb has the problem that i've illustrated ; for which reason do you think that the pcb was connected trought something different  ...? 

0 项奖励
回复

2,174 次查看
GottiLuca
Contributor IV

Dear Mr. Sun,

I have connected on J28 connector with the USB cable supplied with the board.

I've done the same on another new EVK ordered which I can debug without problem.

But the first pcb has the problem that i've illustrated ; for which reason do you think that the pcb was connected trought something different  ...? 

0 项奖励
回复