Prevent external SRAM use

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Prevent external SRAM use

Jump to solution
2,470 Views
adi2Intel
Contributor III

Hi all,

MXRT1050\1052

I'm sorry if this question was asked before, couldn't find the answer .

What should be set in the SDK to avoid using external RAM?

 

Thanks,

Adi

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,462 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @adi2Intel ,

   If you don't want to use the external SDRAM, and you are using the SDK code for RT1050\2, it is very easy, just set:

XIP_BOOT_HEADER_DCD_ENABLE=0

kerryzhou_0-1647835917796.png

And delete the SDRAM memory from 0X80000000

kerryzhou_1-1647835953489.png

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

 

View solution in original post

0 Kudos
Reply
2 Replies
2,463 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @adi2Intel ,

   If you don't want to use the external SDRAM, and you are using the SDK code for RT1050\2, it is very easy, just set:

XIP_BOOT_HEADER_DCD_ENABLE=0

kerryzhou_0-1647835917796.png

And delete the SDRAM memory from 0X80000000

kerryzhou_1-1647835953489.png

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

 

0 Kudos
Reply
2,005 Views
larrydemuth
Contributor III

I was just wondering how we know what defines to use in this? Is there documentation that tells what they are and what they do?

0 Kudos
Reply