Peripheral access from both cores

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Peripheral access from both cores

Jump to solution
1,501 Views
Mysterion
Contributor II

Dear sirs,

does the i.MXRT117x allow access to any peripheral from both cores, or is the access limited to the peripherals each core is connected to directly?

In first case: is there any drawback, like slowing down the M7 AHB bus when accessing FlexSPI from the M4 core?

 

Tags (1)
0 Kudos
Reply
1 Solution
1,482 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Mysterion,

Outside some GPIOs and the MMCAU there's not much restrictions about the peripherals. You can check this in the chapter 3.3.

About the performance, the FLEXIO limit frequency is independent from each core so the performance would only be affected in the data processing.

Best Regards,
Alexis Andalon

View solution in original post

0 Kudos
Reply
1 Reply
1,483 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Mysterion,

Outside some GPIOs and the MMCAU there's not much restrictions about the peripherals. You can check this in the chapter 3.3.

About the performance, the FLEXIO limit frequency is independent from each core so the performance would only be affected in the data processing.

Best Regards,
Alexis Andalon

0 Kudos
Reply