PWM using Flexio_PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM using Flexio_PWM

2,521 Views
ManikantaRobbi
Contributor II

Hi,

I am trying to generate a PWM signal with Frequency=20Hz and DC=14%.I imported the flexio_pwm example from SDK which uses generates PWM at frequency=47MHz using kCLOCK_Root_Flexio2, i.e. 24Mhz.

But my application requires very low frequency <100Hz, when I try to change in Clock Configuration tool, it is showing error:

ManikantaRobbi_0-1706176728175.png

and also I tried setting to 100kHz, now clock configuration updated fine but in my source code, 

ManikantaRobbi_1-1706176800257.png

there is a calculation of sum, lower & upper values which set the timer compare. when I'm using 100kHz as clock frequency, I'm getting value more than uint32_t.

Is there any other provision to use clock configuration or other method to figure out the issue.

 

 

Thanks & regards,

Manikanta Robbi.

0 Kudos
Reply
4 Replies

2,469 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

You need to change the SOC domain voltage set point.

_Leo__0-1706573048920.png

Hope it helps you.

Have a nice day!

0 Kudos
Reply

2,466 Views
ManikantaRobbi
Contributor II

Thanks @_Leo_ ,

For the information, I had tried changing SOC Domain Voltage Set Point,  but not able to set 100KHz for FlexIO2 Clock root. Can you please guide steps to change and provide Application note or Reference manual.

 

Thanks & Regards,

Manikanta Robbi.

0 Kudos
Reply

2,460 Views
ManikantaRobbi
Contributor II

Hi, 

As per guidance, I changed SOC Domain voltage point: Normal. And changed so configurations like

1)creating new functional group.

2)Enabling SYS_PLL_DIV5_CLK.

But the problem arises, when flashing code to MCU (resetting) or Not able to enter into Debug mode, Why? Is there any effect changing clock from 48Mhz to any PLL (ARM, or any similar options mention in the clock tree) may impact code flashing into memory.

ManikantaRobbi_0-1706608406455.png

 

 

Thanks & Regards,

Manikanta Robbi.

0 Kudos
Reply

2,451 Views
ManikantaRobbi
Contributor II

Hi @_Leo_ ,

I had found that clock is changing fine when we select: 48MHZ RC OSC

ManikantaRobbi_0-1706615364716.png

 

 

But the issue, when I configure with:SYS_PLL1_DIV5(making as active)

ManikantaRobbi_1-1706615443440.png

Note: this SYS_PLL is chosen from: External 24MHz Crystal

ManikantaRobbi_2-1706615541300.png

Why I'm not able to get frequency configured using PLL (by opting OSC_24MHz).

 

 

Thanks,

Manikanta Robbi.

 

0 Kudos
Reply