Hi community people
We are using IMXRT1020 EVK board , We want to test flashing with PE Micro Universal , Can some one guide on the board settings
We have IMXRT1020 EVK , PE Micro Universal JTAG
Connected the JTAG 20 pin connector to J16 of the board ,
Checked that jumpers J27 and J28 are off (they are on by default when boards ship from the factory) to ensure SWD signals are disconnected from the OpenSDA microcontroller.
In the IDE we have selected PE Micro in Debug configuration
We are facing the below error , Please suggest the proper settings
Hi Naren,
Yes, you can disconnect J27 and J28, then connect Multilink Universal to J16. That should be enough.
https://community.nxp.com/message/1044022?commentID=1044022#comment-1044022
Maybe you can try to update Multilink firmware.
http://www.pemicro.com/downloads/download_file.cfm?download_id=346
Here is other people who ask similar question.
https://community.nxp.com/message/1163806?commentID=1163806#comment-1163806
Regards,
Jing
Thanks Jing Pan ,
That was helpful