Optimized ADC configuration for RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Optimized ADC configuration for RT1060

Jump to solution
1,904 Views
kurt_staubli
Contributor III

We use MIMXRT1060CVJ45A as a motor controller. I try to optimize ADC parameters used for current sense to increase speed with the same accuracy.

I qualify accuracy by calculate standard deviation of many samples.

The actual parameters are the following:

 

 

 

...
adc_config_t k_adcConfig;                                                                                                                                         
ADC_GetDefaultConfig(&k_adcConfig);                                                                                                                               
k_adcConfig.enableOverWrite = true;                                                                                                                               
k_adcConfig.enableHighSpeed = true;                                                                                                                               
k_adcConfig.enableLongSample = false;                                                                                                                             
k_adcConfig.samplePeriodMode = kADC_SamplePeriodShort4Clocks;                                                                                                     
k_adcConfig.enableAsynchronousClockOutput = false; // Has to be false, see https://community.nxp.com/t5/i-MX-Processors/ADC-SyncMode-Noise/m-p/992934             
k_adcConfig.clockSource = kADC_ClockSourceIPG;                                                                                                                    
k_adcConfig.clockDriver = kADC_ClockDriver4;      
...                                                                                                                                                                                                                                                                                                                                            

 

 

 

When I decrease samplePeriodMode, I decrease accuracy significantly and speed is increased only a bit (since this parameter affects only sampling, not conversion).

When I decrease clockDriver, I increase ADC's clock frequency (FADCK). If I set it to kADC_ClockDriver2, FADCK increases from 33MHz to 66MHz. Speed is improved significantly and accuracy is even a bit better. But NXP limits FADCK to 4...40 MHz for our CPU.

My question:

How does a violation of the limits of FADCK manifest itself?

Are there any other parameters for improving speed without affecting accuracy?

0 Kudos
Reply
1 Solution
1,888 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Kurt,

Regarding your questions:

1. Please check this note from the RM:

The ADCK frequency must be between fADCK minimum and fADCK maximum to meet ADC specifications.

This will mean that we will not be able to guarantee ADC measurements and specification if clock is outside recommended range.

2. As you mentioned the limit is 40 MHz so if what you need is to increase FADCK then I am afraid it is not recommended as it could cause unpredicted behavior.

Best regards,

Felipe

View solution in original post

0 Kudos
Reply
2 Replies
1,889 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Kurt,

Regarding your questions:

1. Please check this note from the RM:

The ADCK frequency must be between fADCK minimum and fADCK maximum to meet ADC specifications.

This will mean that we will not be able to guarantee ADC measurements and specification if clock is outside recommended range.

2. As you mentioned the limit is 40 MHz so if what you need is to increase FADCK then I am afraid it is not recommended as it could cause unpredicted behavior.

Best regards,

Felipe

0 Kudos
Reply
1,875 Views
kurt_staubli
Contributor III

Hi Felipe

I almost expected this answer

So I cannot improve ADC's performance.

Thanks anyway.

Best regards

Kurt

0 Kudos
Reply