Hi,
IMXRT1021 boot informations are provided in section 8.1 and page 287 of the referance manual. (IMXRT1020RM.pdf)
Peripheral Instance Port(IO function) PAD Mode
LPUART 1 LPUART1_TX GPIO_AD_B0_12 ALT2
LPUART1_RX GPIO_AD_B0_13 ALT2
But, LPUART1 peripheral is not found in the defined pads.
We ask for help with the correct pads for the LPUART1 peripheral for boot the device.
Hello Bora,
Table 8-1 of the reference manual it's wrong, thanks for catching that! I already reported this and it will be fixed in future releases.
LPUART1_RX and LPUART1_TX according to the IOMUX Controller are located in pins GPIO_AD_B0_07 and GPIO_AD_B0_06.
Hope it helps!
Victor.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------