Using an IMXRT1062 on an IMXRT1060 Evaluation kit, I'm trying to run the code from a NOR flash memory (XIP). I noticed if I disable the prefetcher (AHBCR->PREFETCHEN = 0), the code runs slightly faster (about 12% to be exact). I am a bit confused as I expect the opposite for disabling the prefetch. So can someone explain in what conditions can this happen or what am I doing wrong?
The flash memory configuration is as follows:
static const FlexSPINorConfig __attribute__((section(".boot_hdr.conf"), used)) g_flash_config ={.memConfig = {.tag = FLEXSPI_CFG_BLK_TAG,.version = FLEXSPI_CFG_BLK_VERSION,.readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackFromDqsPad,.csHoldTime = 3u,.csSetupTime = 3u,.columnAddressWidth = 0u,.configCmdEnable = 0u,.controllerMiscOption = (1 << kFlexSpiMiscOffset_SafeConfigFreqEnable),.deviceType = kFlexSpiDeviceType_SerialNOR,.sflashPadType = kSerialFlash_4Pads,.serialClkFreq = kFlexSpiSerialClk_133MHz,.lutCustomSeqEnable = 0u,.sflashA1Size = 0x00800000u, /* 8MB/64Mbit */.lookupTable ={// 0 Fast read sequence[0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD,0x18),[1] = FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),[2] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[3] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 1 Read Status sequence[4] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x04),[5] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[6] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[7] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 2 Reserved[8] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[9] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[10] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[11] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 3 Write Enable sequence[12] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, 0, 0),[13] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[14] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[15] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 4 Reserved[16] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[17] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[18] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[19] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 5 erase sector sequence[20] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x20, RADDR_SDR, FLEXSPI_1PAD, 0x18),[21] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[22] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[23] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 6 Reserved[24] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[25] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[26] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[27] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 7 Reserved[28] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[29] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[30] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[31] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 8 Reserved[32] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD8, RADDR_SDR, FLEXSPI_1PAD, 0x18),[33] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[34] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[35] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 9 page program sequence[36] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02, RADDR_SDR, FLEXSPI_1PAD, 0x18),[37] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x04, STOP, 0, 0),[38] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[39] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 10 Reserved[40] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[41] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[42] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[43] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 11 chip erase sequence[44] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60, STOP, 0, 0),[45] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[46] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[47] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 12 Reserved[48] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[49] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[50] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[51] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 13 Reserved[52] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[53] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[54] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[55] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 14 Reserved[56] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[57] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[58] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[59] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),// 15 Reserved[60] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[61] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[62] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),[63] = FLEXSPI_LUT_SEQ(STOP, 0, 0, STOP, 0, 0),},},.pageSize = 256,.sectorSize = 4096,.ipcmdSerialClkFreq = kFlexSpiSerialClk_30MHz,.isUniformBlockSize = 0,.serialNorType = 0,.needExitNoCmdMode = 0,.halfClkForNonReadCmd = 0,.needRestoreNoCmdMode = 0,.blockSize = 0x10000,};
已解决! 转到解答。
Hi Kamran Farhangi ,
Sorry for reply late.
I do the similar testing as you did (Fig 1), comparing the executing time of mbedtls library function between disabling and enabling AHB Read Prefetch feature circumstances, however, I find the result is versus to your previous result.
I've attached the testing demo, maybe you can give a try.
Fig 1
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi jeremyzhou,
Sorry for the late reply,
The code that I had mentioned earlier is a part of a bigger project and I can not upload the whole project here. I isolated the part that is related to my question and attached to this reply. You probably need to include the cmake file and possibly change a few thing so that it compiles on your setup. Thank you in advance.
Hi Kamran Farhangi ,
Sorry for reply late.
I do the similar testing as you did (Fig 1), comparing the executing time of mbedtls library function between disabling and enabling AHB Read Prefetch feature circumstances, however, I find the result is versus to your previous result.
I've attached the testing demo, maybe you can give a try.
Fig 1
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks, then I guess something else is happening while I'm performing this test, like some thread switching in the background or so, because I run this example inside an RTOS and with a minimized number of background tasks. Now I know that the prefetcher does increase the performance in an example like this.
Hi jeremyzhou,
Thank you for your reply. To test the code execution time, I am using a jpeg decoder and I have made 8 copies of it with different function names so that it is big enough to fill i-cache between iterations. Here is the code:
while(true)
{
uint32_t maxNs = 0;
uint32_t minNs = UINT32_MAX;
uint64_t SumNs = 0;
uint32_t count = 1000;
for(uint32_t i = 0; i < count; i++)
{
uint32_t start = DWT->CYCCNT;
dec decoder;
decoder.decode(pic, sizeof(pic));
dec2 decoder2;
decoder2.decode(pic, sizeof(pic));
dec3 decoder3;
decoder3.decode(pic, sizeof(pic));
dec4 decoder4;
decoder4.decode(pic, sizeof(pic));
dec5 decoder5;
decoder5.decode(pic, sizeof(pic));
dec6 decoder6;
decoder6.decode(pic, sizeof(pic));
dec7 decoder7;
decoder7.decode(pic, sizeof(pic));
dec8 decoder8;
decoder8.decode(pic, sizeof(pic));
uint32_t end = DWT->CYCCNT;
volatile uint32_t ns = GetNs(start, end);
if(ns > maxNs)
maxNs = ns;
if(ns < minNs)
minNs = ns;
SumNs += ns;
}
uint32_t mean = SumNs / count;
printf("Timings: Mean = %u us, Min = %u us, Max = %u us", mean / 1000, minNs / 1000,
maxNs / 1000);
}When the prefetch bit is set, the mean execution time (the one that is printed out) is about 2372 microseconds. Then if I set a breakpoint somewhere outside the for loop and set the AHBCR->PREFETCHEN register to zero, the code execution time will be 2090 microseconds, about 88% of the time with prefetcher being on. This behavior is pretty consistent and if I set AHBCR->PREFETCHEN to one again, it will jump up to 2372 microseconds again.
Hi Kamran Farhangi ,
Thanks for your reply.
I was wondering if you can share the complete demo, as I'd like to do testing on my site, in further, I'd like to suggest you run the mbedtls_selftest which performs a variety of cryptographic algorithms to double confirm the aforementioned phenomenon.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kamran Farhangi ,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Before answering your question, I'd like to get more information, so I was wondering if you can present the testing steps you did in detail.
Looking forward to your reply.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------