Hello Patrick,
Hope you are doing well.
Yes, you are able to connect two flash devices to port A. Please review section 27.5.3 of the reference manual here it is described the considerations to take when connecting two flash devices. There are two FlexSPI interface ports (A port and B port). Each port supports 2 flash devices by providing 2 chip select outputs.

Based on your previous thread your timings are fine, since they should both be working with the same configurations in order for both of them to be attached to the same port.
In addition, I'd recommend to check this post that answers some questions that come up with this configuration.
https://community.nxp.com/message/1274847
Best Regards,
Sabina
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------