Multiple ADCs using DMA on the RT1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple ADCs using DMA on the RT1020

2,234 Views
tjhaeser
Contributor I

On the RT1020, is it possible to sample multiple ADCs at the same time using DMA? If so, how many different ADC pins at the same time? I couldn't find anything conclusive in the manual.

I'd be immensely grateful for any nudge in the right direction.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,039 Views
igorpadykov
NXP Employee
NXP Employee

Hi TJ

seems this is possible as described in Chapter 15 ADC External Trigger Control (ADC_ETC)

i.MXRT1020 Reference Manual :

Capable of triggering dual ADC in SyncMode or AsyncMode:
• In SyncMode ADC1 and ADC2 are controlled by the same trigger source.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,039 Views
tjhaeser
Contributor I

Hello, thanks for your input.

The issue is that we need to sample 6 ADC *pins* at the same time. The data is very time sensitive, so there should be next to no delay between the samples. We've tried a number of things, but so far were unable to do this.

0 Kudos
Reply

2,039 Views
igorpadykov
NXP Employee
NXP Employee

i.MXRT1050 ADC is a successive approximation ADC block, so by design

it is not possible to perform adc conversion simultaneously on all inputs. Conversion

is perfomed in sequence: first channel, then next, e.t.c.

Best regards
igor

0 Kudos
Reply