Mimxrt1060-EVK and Zephyr's LED_blinky

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mimxrt1060-EVK and Zephyr's LED_blinky

1,693 Views
prayrit
Contributor I

Hello everyone, 

I am using the MiMXRT1060-EVK and am currently trying to flash Zephyr's LED_blinky example. I have been on the Zephyr thread and have seen some issues with this board and the LED_blinky. It seems that LED0 is not set to the proper LED_GPIO. If anyone has any idea how to move forward or has any idea where to look to fix the problem please reply!!

Thanks

Pray

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,608 Views
dleach
NXP Employee
NXP Employee

The problem has been addressed and is in the pending Release v2.4. 

0 Kudos
Reply

1,624 Views
dleach
NXP Employee
NXP Employee

Pray,

I have narrowed down which changeset broke the support. We will work on getting a fix in next week.

The broken code is sensitive to the sequence on how you test it so if you go back to release 2.2 it works fine and if you download broken code without powering off the board it would continue to work.

We can engage on the Zephyr slack for more information.

David

0 Kudos
Reply

1,624 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Pray, 

I'm not aware of the example that you mentioned, could you please tell me where did you get this example?

Regards, 

Victor 

0 Kudos
Reply