Need help with evkmimxrt1180_ecat_digital_io_cm33/cm7 example for MIMXRT1180-EVK.
I can compile, flash and emulate the demo using MCUXpresso IDE and the SDK, but it seems do not correct configure the phys...
Should a working firmware turn on a led on the RJ connectors after hw init?
Can the EVK be used as is with the demo or I must change some jumper position / resistors?
Is it correct that the EVK used as is should work well with the demo using Phy0/Phy4 in RMII mode?
Any useful information about the topic will be very appreciated!