Hi team,
For MIMXRT1176CVM8A, 20 pin 2.54mm connector is used for JTAG as per reference schematics. This corresponds to Port B of Multilink Universal programmer as shown below.
My query: Can we go for the "Port G" of Multilink universal programmer (shown below) so that we can have reduced size JTAG connector on the PCB.??
Solved! Go to Solution.
thanks for the quick support
Hi @Yogesh96 ,
Sure, you can use the 10 pin SWD interface, as the RT1170 can support both the JTAG and SWD interface.
You can use this interface:
SWD just need the SWD_CLK, SWD_DATA, Reset, VDD, GND.
So, you can use PORT G, just make sure your designed PCB have the same interface, which need to connect the SWD signal sequence correctly to the debugger.
Wish it helps you!
If you still have question about it, please kindly let me know.
If your question is solved, please help me to mark the correct answer, just to close this case, thanks.
Any new issues, welcome to create the new case.
Best Regards,
kerry