MIMXRT1176CVM8A (MIMXRT1176 Family's)JTAG related query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1176CVM8A (MIMXRT1176 Family's)JTAG related query

Jump to solution
435 Views
Yogesh96
Contributor II

Hi team,

For MIMXRT1176CVM8A, 20 pin 2.54mm connector is used for JTAG as per reference schematics. This corresponds to Port B of Multilink Universal programmer as shown below. 

Yogesh96_0-1713338832760.png

My query: Can we go for the "Port G" of Multilink universal programmer (shown below) so that we can have reduced size JTAG connector on the PCB.??

Yogesh96_1-1713338926090.png

 

0 Kudos
Reply
1 Solution
412 Views
Yogesh96
Contributor II

thanks for the quick support

View solution in original post

0 Kudos
Reply
2 Replies
413 Views
Yogesh96
Contributor II

thanks for the quick support

0 Kudos
Reply
420 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Yogesh96 ,

    Sure, you can use the 10 pin SWD interface, as the RT1170 can support both the JTAG and SWD interface.

    You can use this interface:

kerryzhou_0-1713407826794.png

    SWD just need the SWD_CLK, SWD_DATA, Reset, VDD, GND.

  So, you can use PORT G, just make sure your designed PCB have the same interface, which need to connect the SWD signal sequence correctly to the debugger.

 

Wish it helps you!

If you still have question about it, please kindly let me know.

If your question is solved, please help me to mark the correct answer, just to close this case, thanks.

Any new issues, welcome to create the new case.

Best Regards,

kerry

 

 

0 Kudos
Reply