When trying to update flash LUT, function FLEXSPI_UpdateLUT fails. MCR0->MDIS is set to zero, so module is not disabled:
MCR0 = 0xffffa030,
MCR1 = 0xffffffff,
MCR2 = 0x200001f7,
AHBCR = 0x78,
INTEN = 0x0,
INTR = 0x41,
LUTKEY = 0x5af05af0,
LUTCR = 0x2,
AHBRXBUFCR0 = {0x80000000, 0x80000000, 0x80000000, 0x80000000, 0x80000000, 0x80000000, 0x80000000, 0x80070040},
RESERVED_0 = {0x0 <repeats 32 times>},
FLSHCR0 = {0x2000, 0x0, 0x0, 0x0},
FLSHCR1 = {0x63, 0x10063, 0x10063, 0x10063},
FLSHCR2 = {0x0, 0x900, 0x900, 0x900},
RESERVED_1 = {0xc, 0xc, 0x0, 0xd},
FLSHCR4 = 0x3,
RESERVED_2 = {0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0},
IPCR0 = 0x0,
IPCR1 = 0x10000,
RESERVED_3 = {0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0},
IPCMD = 0x0,
RESERVED_4 = {0x0, 0x0, 0x0, 0x0},
IPRXFCR = 0x1c,
IPTXFCR = 0x1c,
DLLCR = {0x79, 0x100},
RESERVED_5 = {0x2, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0},
MISCCR4 = 0x0,
MISCCR5 = 0x0,
MISCCR6 = 0x0,
MISCCR7 = 0x0,
STS0 = 0x3,
STS1 = 0x0,
STS2 = 0x1353,
AHBSPNDSTS = 0x0,
IPRXFSTS = 0x0,
IPTXFSTS = 0x80007,
RESERVED_6 = {0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0},
RFDR = {0x8b2007dc, 0x0, 0x0, 0x0, 0x8b200712, 0xa304, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x760, 0x0 <repeats 19 times>},
TFDR = {0x0 <repeats 32 times>},
LUT = {0x8b2007fd, 0xa704b306, 0x0, 0x0, 0x4000481, 0x4000400, 0x2001, 0x0, 0x799, 0x0 <repeats 55 times>},
RESERVED_7 = {0x0 <repeats 256 times>},
HMSTRCR = {0x40ffcf, 0xffcf, 0x4f00f, 0x22807f, 0x32f87f, 0x11f87f, 0x0, 0x0},
HADDRSTART = 0x0,
HADDREND = 0x0,
HADDROFFSET = 0x0
Debug sessions gets killed at the instance when code tries to update the LUT:
I haven't found a way to interrogate the processor as debugger disconnects.