MIMXRT1060-EVKB - Dual USB Host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060-EVKB - Dual USB Host

Jump to solution
188 Views
timmek
Contributor II

Hello,

Hardware: MIMXRT1060-EVKB

I found the tutorial (Implementation of Dual USB Host on RT1060 EVK ) describing how to implement two USB Hosts on the development board..

I would like to implement the presented solution on MIMXRT1060-EVKB Board. In MIMXRT1060-EVKB Board User Manual, Rev. 0, 7 January 2022 I found this table:

MIMXRT1060-EVKB Board User Manual, Rev. 0, 7 January 2022.PNG

I run few examples from SDK. I also I used Config Tool to manually add USB Host (USB1 or USB2). In all cases I can plug USB device only to the J47 socket (and the device is powered). But when I plug device in socket J48 it is not working - it is not powered.

How can I enable 5V to the J48 socket and use this socket as USB Host like in the tutorial I mentioned?

0 Kudos
Reply
1 Solution
145 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @timmek,

There is no need to enable J48 with 5V via software. As you can see from the schematic of the RT1060-EVKB, J48 VBUS is already connected to 5V:

EdwinHz_0-1721257670847.png

BR,
Edwin.

View solution in original post

1 Reply
146 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @timmek,

There is no need to enable J48 with 5V via software. As you can see from the schematic of the RT1060-EVKB, J48 VBUS is already connected to 5V:

EdwinHz_0-1721257670847.png

BR,
Edwin.