MCUXpresso_Config_Tools_v8 配置ADC_ETC的触发中断时出现问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso_Config_Tools_v8 配置ADC_ETC的触发中断时出现问题

2,758件の閲覧回数
milo_bai
Contributor II

Hi 你好。

我的项目使用了RT1052芯片,开发环境使用MCUXpreeso 11.2.0_4120,并单独安装了MCUXpresso_Config_Tools_v8,今天在使用ADC_ETC外设配置时出现问题,问题如下图,当我选择XBAR1_TRIG,0作为触发源时,下面的Trigger Group 则一直为0。几天前使用这个工具时还可以显示为4,一切功能都正常,由于这个问题导致我调试突然出现问题,一时找不到问题,后经过代码对比发现这个问题。之后重新安装了MCUXpreeso 11.2.0_4120问题依旧。请问如何解决这个问题,每次代码生成以后都需要手动修改peripherals.c和peripherals.h两个文件中对应的宏定义,使用很麻烦。希望能给个解决办法。

milo_bai_0-1603519358777.png

 

 

0 件の賞賛
返信
3 返答(返信)

2,748件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
建议重新安装MCUXpresso_Config_Tools_v8,我这边没有出现这样的现象。

jeremyzhou_0-1603681257603.png

 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,738件の閲覧回数
milo_bai
Contributor II

非常感谢您的回复,我已经重新安装了MCUXpresso_Config_Tools_v8和MCUXpresso_IDE,这两个地方的问题一样没有解决,请问这两个工具还与系统环境、变量或者默认配置之类的目录等是不是有关系?希望能指导一下解决这个问题。或者怎样能够彻底删除这两个工具,可以类似重新安装一样。

0 件の賞賛
返信

2,733件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
安装与删除MCUXpresso_Config_Tools_v8和MCUXpresso_IDE不需要额外的设置,还有在MCUXpresso IDE中加载了SDK library中的例程后,可以在IDE中加载配置的外设的config Tool,你看看是否也出现上述这种现象,可以的话,你最好截图介绍一下你配置ADC_ETC的步骤。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信