MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller

593件の閲覧回数
yvkrkrishna
Contributor III

Hi,

I am using IMXRT 1050 micro controller and MAX 17260 chip for battery capacity reading.

Now i want to check whether battery is connected or removed.

As per the datasheet i am reading the register "CONFIG REGISTER" it is always coming value as 0x2210

In CONFIG Register(0x1D),

Bit positions:

0th bit  D0 - Ber     (battery Removal)

1st bit  D1 - Bei     (battery Insertion)

Can anyone please guide me how to get the connection or removal status of MAX 17260 battery.

ラベル(1)
0 件の賞賛
返信
1 返信

583件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think you'd better contact Maxim integrated apply for some advice or suggestions, as I'm not familiar with their products.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------