Linking power_mode_switch example and MCUExpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linking power_mode_switch example and MCUExpresso

1,366件の閲覧回数
DK2
Contributor I

Hi,

I' m using a MIMXRT1170-EVKB.

Please tell me about linking power_mode_switch example(dcdc) and MCUExpresso.

My understanding is that clock configration made with MCUExpresso doesn't applied because this example doesn't call BOARD_BootClockRUN().

Is this correct ? 

I want to link them. 

Is there any better way ?

Best regards.

0 件の賞賛
返信
3 返答(返信)

1,348件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DK2,

Indeed, the changes made by Clocks Tool will not immediately apply on the power_mode_switch example, as this example doesn't call the BOARD_BootClockRUN() function. That said, you can always make a call to this function on the main() routine, just like the BOARD_ConfigMPU() or the BOARD_InitPins() functions. This way, the ConfigTools configuration changes that you make will be reflected once the BOARD_BootClockRUN() function is called on main().

BR,
Edwin.

0 件の賞賛
返信

1,337件の閲覧回数
DK2
Contributor I

Thank you for your reply.

I tried the way you mentioned.

I called BOARD_BootClockRUN() after ChipInitConfig().

But program staied at ANATOP_AI_Access() of fsl_anatop_ai.c. 

DK2_0-1705459540021.png

What should I do ?

Best regards.

0 件の賞賛
返信

1,310件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @DK2,

What routine from the BOARD_BootClockRUN() was last called when the ANATOP_AI_Access() caused the CPU to halt? I ask this because the ANATOP_AI_Access routine gets called on several occasions during the BOARD_BootClockRUN, so the ANATOP function does not tell much on its own. Was is the procedure of routines that ended up with the ANATOP halt? (for example BOARD_BootClockRUN() > CLOCK_SetPllBypass() > ANATOP_PllBypass() > ANATOP_AI_Write() > ANATOP_AI_Access() )

BR,
Edwin.

0 件の賞賛
返信