Lab 1. wifi_webconfig_nxp_wireless_RT1060.pdf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lab 1. wifi_webconfig_nxp_wireless_RT1060.pdf

118,463件の閲覧回数
GovindaAjay
Contributor I

During Demo Execution, 

I got the following error.

 

ÇËßc¶oOgcwç—WãK×ÛË×KßWÇ[þWëc¯kÞO
Starting webconfig DEMO
[i] Trying to load data from mflash.
[i] Nothing stored yet
[i] Initializing WiFi connection...
[sdio] Error: Card initialization failed
[wifi_io] Error: SDIO driver init failed.
[wifi] Error: sd_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1
[wlcm] Error: cannot start wlcmgr. unexpected status: 0
[!] Could not initialize WiFi module 3

0 件の賞賛
返信
3 返答(返信)

118,458件の閲覧回数
laserhsu
NXP Employee
NXP Employee

please double check jumpers and make sure wifi module connected to RT well. 

0 件の賞賛
返信

118,452件の閲覧回数
GovindaAjay
Contributor I

I have connected the module exactly how it shows on the lab guide. 

Please have a look at the attached image and suggest if anythings out of place.

Thanks

~~~~~

0 件の賞賛
返信

118,432件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi GovindaAjay,

  I have checked your board jump connection, it is wrong, the lab1 document requred you configure the azurewave jumper settings as

J2[1-2]:Voltage Source Selected to SDIO Host

j11[1-2]:Select SDIO Voltage Level 1.8V

Please check my attached two photos from my side.

I have followed the lab1 document and test it on my side, it totally works, the same result as the document.

So, please test it again.

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------