During Demo Execution,
I got the following error.
ÇËßc¶oOgcwç—WãK×ÛË×KßWÇ[þWëc¯kÞO
Starting webconfig DEMO
[i] Trying to load data from mflash.
[i] Nothing stored yet
[i] Initializing WiFi connection...
[sdio] Error: Card initialization failed
[wifi_io] Error: SDIO driver init failed.
[wifi] Error: sd_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1
[wlcm] Error: cannot start wlcmgr. unexpected status: 0
[!] Could not initialize WiFi module 3
Hi GovindaAjay,
I have checked your board jump connection, it is wrong, the lab1 document requred you configure the azurewave jumper settings as
J2[1-2]:Voltage Source Selected to SDIO Host
j11[1-2]:Select SDIO Voltage Level 1.8V
Please check my attached two photos from my side.
I have followed the lab1 document and test it on my side, it totally works, the same result as the document.
So, please test it again.
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------