We are using Zephyr and the iMXRT1052 LPSPI. I am trying to interface to a device (LTC2986) that requires me to send 7 bytes in a single transfer. The driver does not allow a frame of 56 bits, so I set a frame of 8 bits and I transfer 7 bytes. However, between each 8 bit group there is a "glitch" in the clock. The clock goes high for the last bit and then goes low so fast as the next byte starts, that it appears as a glitch. The last bit in the frame does not get a full clock high time. I spent all day trying different configurations in an attempt to fix this, with no success. Do you have any suggestions?
The driver in use is the NXP fsl_lpspi.c/h.
解決済! 解決策の投稿を見る。
We are using 8 bit frames. The problem was that we needed to send 7 such frames. We are not attempting to send 7 bits, we are sending 7 bytes.
I fixed the problem after my colleague found some variables that can be set in the device tree to affect the operation of the driver. There are 3 variables, sck-pcs-delay, pcs-sck-delay, and transfer-delay.
pcs-sck-delay sets the number of ns from chip-select active to sck active at the beginning of the transfer.
sck-pcs-delay sets the number of ns from sck inactive to chip-select inactive at the end of the transfer.
transfer-delay sets the number of ns between frames during the transfer.
Since we were not using these variables at first we were getting 0 ns between frames during the transfer, which appeared as glitches on the scope. I set transfer delay to 1000 and it put 1 us between frames which made the glitches disappear, and now everything works fine.
Thank you for your interest and help.
Hi @kk7xo ,
To the RT1050 SPI, the minimum frame size is 8bits, so your 7 bit can't be supported.
If you want to use 8bit*7, and you want each byte is not delayed, I suggest you use the DMA, that transfer is quick, and each byte is near, you can try it on your side.
Best Regards,
Kerry
We are using 8 bit frames. The problem was that we needed to send 7 such frames. We are not attempting to send 7 bits, we are sending 7 bytes.
I fixed the problem after my colleague found some variables that can be set in the device tree to affect the operation of the driver. There are 3 variables, sck-pcs-delay, pcs-sck-delay, and transfer-delay.
pcs-sck-delay sets the number of ns from chip-select active to sck active at the beginning of the transfer.
sck-pcs-delay sets the number of ns from sck inactive to chip-select inactive at the end of the transfer.
transfer-delay sets the number of ns between frames during the transfer.
Since we were not using these variables at first we were getting 0 ns between frames during the transfer, which appeared as glitches on the scope. I set transfer delay to 1000 and it put 1 us between frames which made the glitches disappear, and now everything works fine.
Thank you for your interest and help.
Thanks for posting the solution, it has helped me alot!
I cannot believe the driver doesn't default to a sane value when transfer-delay is absent, its a really bad design by NXP!