LPSPI PCS behavior on RT105x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI PCS behavior on RT105x

4,413 Views
ryanshuttlewort
Contributor IV

Hello, I am using IAR with an RT1050 SDK, version  2.3.0 (2017-11-16).  I am having a strange issue with the LPSPI chip select (PCS) when sending data.  I am trying to achieve what I would call ideal CS behavior and that is:

  • Chip select should drop
  • 5 words should get clocked out and chip select should not rise between words
  • Chip select should rise after the last word is clocked

So far the only way I have been able to achieve this is demonstrated with the following simple example (which seems a bit silly)

LPSPI Setup

LPSPI_MasterGetDefaultConfig(&masterConfig);

masterConfig.baudRate = pCtx->baudRate;
masterConfig.bitsPerFrame                  = 16;
masterConfig.cpol                          = kLPSPI_ClockPolarityActiveHigh;
masterConfig.cpha                          = kLPSPI_ClockPhaseSecondEdge;
masterConfig.direction                     = kLPSPI_MsbFirst;
masterConfig.pcsToSckDelayInNanoSec        = 100;
masterConfig.lastSckToPcsDelayInNanoSec    = 100;
masterConfig.betweenTransferDelayInNanoSec = 0;
masterConfig.whichPcs                      = kLPSPI_Pcs0;
masterConfig.pcsActiveHighOrLow            = kLPSPI_PcsActiveLow;

LPSPI_MasterInit(LPSPI3, &masterConfig, LPSPI_CLOCK_FREQ);

LPSPI TX

/*! Just a low-overhead LPSPI TX routine */
#define RAW_LPSPI_TX(spi, pBuf, n)     \
    do {                               \
        for (int _i = 0; _i < n; _i++) \
        {                              \
            spi->TDR = pBuf[_i];       \
        }                              \
    } while (0)

for (i = 0; i < 5; i++)
{  
     LPSPI3->TCR |= (LPSPI_TCR_CONT_MASK | LPSPI_TCR_CONTC_MASK);
     RAW_LPSPI_TX(LPSPI3, buf, 5);
     LPSPI3->TCR &= ~(LPSPI_TCR_CONT_MASK | LPSPI_TCR_CONTC_MASK       
}

It seems I have to begin the transaction in one mode and terminate with another.  If I don't do the above wrapping I either get chip select rises between words or a chip select that will drop but never rise once the words are transmitted.  I have seen a similar issue in this post

Could someone please recommend a setup that can be performed once and have LPSPI CS behave "ideally" from then on?

Thanks.

Labels (1)
5 Replies

2,977 Views
HeMyFAE
NXP Employee
NXP Employee

HI Ryan,

Beside the SDK that you downloaded, there is an extended example code (YUri's previous response) that include LPSPI demo code.

Unfortunately, the code is supported only on Iar, keil and GCC tool  at the moment. MCUXpresso support will be released by the end of March.

We do have access to early alpha/beta package that support MCUXpresso but you will have to be a guinea  pig if you want it.

I  played with the demo code below and the CS signal does seem to encompass the entire data frame.

After you unzip the example code, please follow the instruction  in the attached pdf file .

It will tell you how to copy each project into the root of KSDK folder structure and then you can recompile.

Basically, user only needs to be copy whatever under the top level folder of certain example to the SDK root, then open the project file in the copied folder. Now the examples are ready to be used..
For example, WiFi_QCA, there’re two folders (Boards and Middleware) in it:
Then these two folders need to be copied to the SDK root directory(where there are also boards and middleware directory):
It will be merged, then open the project file in the copied example folder.

2,977 Views
jackking
Senior Contributor I

Ryan,

Do you have an example project you can share for setting up LPSPI on the rt1052?  I don't find any samples for the lpspi driver in the sdk.  I am trying to use an spi tft module (ili9341) with the 1052.

0 Kudos
Reply

2,977 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

2,977 Views
ryanshuttlewort
Contributor IV

Hello Jack, I had to ask an FAE for an LPSPI example.  I don't seem to be able to attach a file in this editor so here is the code.

lpspi_interrupt.c

/*
 * Copyright (c) 2013 - 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 *
 * Redistribution and use in source and binary forms, with or without modification,
 * are permitted provided that the following conditions are met:
 *
 * o Redistributions of source code must retain the above copyright notice, this list
 *   of conditions and the following disclaimer.
 *
 * o Redistributions in binary form must reproduce the above copyright notice, this
 *   list of conditions and the following disclaimer in the documentation and/or
 *   other materials provided with the distribution.
 *
 * o Neither the name of the copyright holder nor the names of its
 *   contributors may be used to endorse or promote products derived from this
 *   software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
 * WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
 * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR
 * ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
 * LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON
 * ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
 * SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "fsl_lpspi.h"
#include "board.h"

#include "fsl_common.h"
#include "pin_mux.h"
#if ((defined FSL_FEATURE_SOC_INTMUX_COUNT) && (FSL_FEATURE_SOC_INTMUX_COUNT))
#include "fsl_intmux.h"
#endif
/*******************************************************************************
* Definitions
******************************************************************************/
/* Master related */
#define EXAMPLE_LPSPI_MASTER_BASEADDR (LPSPI3)
#define EXAMPLE_LPSPI_MASTER_IRQN (LPSPI3_IRQn)
#define EXAMPLE_LPSPI_MASTER_IRQHandler (LPSPI3_IRQHandler)

#define EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT (kLPSPI_Pcs0)
#define EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER (kLPSPI_MasterPcs0)

/* Slave related */
#define EXAMPLE_LPSPI_SLAVE_BASEADDR (LPSPI1)
#define EXAMPLE_LPSPI_SLAVE_IRQN (LPSPI1_IRQn)
#define EXAMPLE_LPSPI_SLAVE_IRQHandler (LPSPI1_IRQHandler)

#define EXAMPLE_LPSPI_SLAVE_PCS_FOR_INIT (kLPSPI_Pcs0)
#define EXAMPLE_LPSPI_SLAVE_PCS_FOR_TRANSFER (kLPSPI_SlavePcs0)

/* Select USB1 PLL PFD0 (720 MHz) as lpspi clock source */
#define EXAMPLE_LPSPI_CLOCK_SOURCE_SELECT (1U)
/* Clock divider for master lpspi clock source */
#define EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER (7U)

#define EXAMPLE_LPSPI_CLOCK_FREQ \
    (CLOCK_GetFreq(kCLOCK_Usb1PllPfd0Clk) / (EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER + 1U))

#define EXAMPLE_LPSPI_MASTER_CLOCK_FREQ EXAMPLE_LPSPI_CLOCK_FREQ
#define EXAMPLE_LPSPI_SLAVE_CLOCK_FREQ EXAMPLE_LPSPI_CLOCK_FREQ

#define TRANSFER_SIZE (512U)        /*! Transfer dataSize .*/
#define TRANSFER_BAUDRATE (500000U) /*! Transfer baudrate - 500k */

/*******************************************************************************
* Prototypes
******************************************************************************/
/* LPSPI user callback */
void LPSPI_SlaveUserCallback(LPSPI_Type *base, lpspi_slave_handle_t *handle, status_t status, void *userData);
void LPSPI_MasterUserCallback(LPSPI_Type *base, lpspi_master_handle_t *handle, status_t status, void *userData);

/*******************************************************************************
* Variables
******************************************************************************/
uint8_t masterRxData[TRANSFER_SIZE] = {0};
uint8_t masterTxData[TRANSFER_SIZE] = {0};
uint8_t slaveRxData[TRANSFER_SIZE] = {0};
uint8_t slaveTxData[TRANSFER_SIZE] = {0};

volatile uint32_t slaveTxCount;
volatile uint32_t slaveRxCount;
uint8_t g_slaveRxWatermark;
uint8_t g_slaveFifoSize;

volatile uint32_t masterTxCount;
volatile uint32_t masterRxCount;
uint8_t g_masterRxWatermark;
uint8_t g_masterFifoSize;

volatile bool isSlaveTransferCompleted = false;
volatile bool isMasterTransferCompleted = false;

/*******************************************************************************
* Code
******************************************************************************/
void LPSPI_SlaveUserCallback(LPSPI_Type *base, lpspi_slave_handle_t *handle, status_t status, void *userData)
{
    if (status == kStatus_Success)
    {
        PRINTF("This is LPSPI slave transfer completed callback. \r\n");
        PRINTF("It's a successful transfer. \r\n\r\n");
    }
    else if (status == kStatus_LPSPI_Error)
    {
        PRINTF("This is LPSPI slave transfer completed callback. \r\n");
        PRINTF("Error occured in this transfer. \r\n\r\n");
    }
    else
    {
        __NOP();
    }

    isSlaveTransferCompleted = true;
}

void LPSPI_MasterUserCallback(LPSPI_Type *base, lpspi_master_handle_t *handle, status_t status, void *userData)
{
    isMasterTransferCompleted = true;
}

void EXAMPLE_LPSPI_SLAVE_IRQHandler(void)
{
    if (slaveRxCount < TRANSFER_SIZE)
    {
        while (LPSPI_GetRxFifoCount(EXAMPLE_LPSPI_SLAVE_BASEADDR))
        {
            slaveRxData[slaveRxCount] = LPSPI_ReadData(EXAMPLE_LPSPI_SLAVE_BASEADDR);
            slaveRxCount++;

            if (slaveTxCount < TRANSFER_SIZE)
            {
                LPSPI_WriteData(EXAMPLE_LPSPI_SLAVE_BASEADDR, slaveTxData[slaveTxCount]);
                slaveTxCount++;
            }
            if (slaveRxCount == TRANSFER_SIZE)
            {
                break;
            }
        }
    }

    /*Update rxWatermark. There isn't RX interrupt for the last datas if the RX count is not greater than rxWatermark.*/
    if ((TRANSFER_SIZE - slaveRxCount) <= g_slaveRxWatermark)
    {
        EXAMPLE_LPSPI_SLAVE_BASEADDR->FCR =
            (EXAMPLE_LPSPI_SLAVE_BASEADDR->FCR & (~LPSPI_FCR_RXWATER_MASK)) |
            LPSPI_FCR_RXWATER(((TRANSFER_SIZE - slaveRxCount) > 1) ? ((TRANSFER_SIZE - slaveRxCount) - 1U) : (0U));
    }

    /* Check if remaining receive byte count matches user request */
    if ((slaveRxCount == TRANSFER_SIZE) && (slaveTxCount == TRANSFER_SIZE))
    {
        isSlaveTransferCompleted = true;
        /* Disable interrupt requests */
        LPSPI_DisableInterrupts(EXAMPLE_LPSPI_SLAVE_BASEADDR, kLPSPI_RxInterruptEnable);
    }
    /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping
      exception return operation might vector to incorrect interrupt */
#if defined __CORTEX_M && (__CORTEX_M == 4U)
    __DSB();
#endif
}

void EXAMPLE_LPSPI_MASTER_IRQHandler(void)
{
    if (masterRxCount < TRANSFER_SIZE)
    {
        /* First, disable the interrupts to avoid potentially triggering another interrupt
        * while reading out the RX FIFO as more data may be coming into the RX FIFO. We'll
        * re-enable the interrupts EXAMPLE_LPSPI_MASTER_BASEADDRd on the LPSPI state after reading out the FIFO.
        */
        LPSPI_DisableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_RxInterruptEnable);

        while (LPSPI_GetRxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR))
        {
            /*Read out the data*/
            masterRxData[masterRxCount] = LPSPI_ReadData(EXAMPLE_LPSPI_MASTER_BASEADDR);

            masterRxCount++;

            if (masterRxCount == TRANSFER_SIZE)
            {
                break;
            }
        }

        /* Re-enable the interrupts only if rxCount indicates there is more data to receive,
        * else we may get a spurious interrupt.
        * */
        if (masterRxCount < TRANSFER_SIZE)
        {
            /* Set the TDF and RDF interrupt enables simultaneously to avoid race conditions */
            LPSPI_EnableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_RxInterruptEnable);
        }
    }

    /*Update rxWatermark. There isn't RX interrupt for the last datas if the RX count is not greater than rxWatermark.*/
    if ((TRANSFER_SIZE - masterRxCount) <= g_masterRxWatermark)
    {
        EXAMPLE_LPSPI_MASTER_BASEADDR->FCR =
            (EXAMPLE_LPSPI_MASTER_BASEADDR->FCR & (~LPSPI_FCR_RXWATER_MASK)) |
            LPSPI_FCR_RXWATER(((TRANSFER_SIZE - masterRxCount) > 1) ? ((TRANSFER_SIZE - masterRxCount) - 1U) : (0U));
    }

    if (masterTxCount < TRANSFER_SIZE)
    {
        while ((LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) < g_masterFifoSize) &&
               (masterTxCount - masterRxCount < g_masterFifoSize))
        {
            /*Write the word to TX register*/
            LPSPI_WriteData(EXAMPLE_LPSPI_MASTER_BASEADDR, masterTxData[masterTxCount]);
            ++masterTxCount;

            if (masterTxCount == TRANSFER_SIZE)
            {
                break;
            }
        }
    }

    /* Check if we're done with this transfer.*/
    if ((masterTxCount == TRANSFER_SIZE) && (masterRxCount == TRANSFER_SIZE))
    {
        isMasterTransferCompleted = true;
        /* Complete the transfer and disable the interrupts */
        LPSPI_DisableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_AllInterruptEnable);
    }
    /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping
      exception return operation might vector to incorrect interrupt */
#if defined __CORTEX_M && (__CORTEX_M == 4U)
    __DSB();
#endif
}

/*!
* @brief Main function
*/
int main(void)
{
    BOARD_InitPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    /*Set clock source for LPSPI*/
    CLOCK_SetMux(kCLOCK_LpspiMux, EXAMPLE_LPSPI_CLOCK_SOURCE_SELECT);
    CLOCK_SetDiv(kCLOCK_LpspiDiv, EXAMPLE_LPSPI_CLOCK_SOURCE_DIVIDER);


    PRINTF("LPSPI functional interrupt example start.\r\n");
    PRINTF("This example use one lpspi instance as master and another as slave on one board.\r\n");
    PRINTF("Master uses interrupt way and slave uses interrupt way.\r\n");
    PRINTF(
        "Note that some LPSPI instances interrupt is in INTMUX ,"
        "you should set the intmux when you porting this example accordingly \r\n");

    PRINTF("Please make sure you make the correct line connection. Basically, the connection is: \r\n");
    PRINTF("LPSPI_master -- LPSPI_slave   \r\n");
    PRINTF("   CLK      --    CLK  \r\n");
    PRINTF("   PCS      --    PCS \r\n");
    PRINTF("   SOUT     --    SIN  \r\n");
    PRINTF("   SIN      --    SOUT \r\n");

    uint32_t errorCount;
    uint32_t i;
    lpspi_master_config_t masterConfig;
    lpspi_slave_config_t slaveConfig;
    uint32_t whichPcs;
    uint8_t txWatermark;

    /*Set up the transfer data*/
    for (i = 0; i < TRANSFER_SIZE; i++)
    {
        masterTxData[i] = i % 256;
        masterRxData[i] = 0;

        slaveTxData[i] = ~masterTxData[i];
        slaveRxData[i] = 0;
    }

    /*Master config*/
    masterConfig.baudRate = TRANSFER_BAUDRATE;
    masterConfig.bitsPerFrame = 8;
    masterConfig.cpol = kLPSPI_ClockPolarityActiveHigh;
    masterConfig.cpha = kLPSPI_ClockPhaseFirstEdge;
    masterConfig.direction = kLPSPI_MsbFirst;

    masterConfig.pcsToSckDelayInNanoSec = 1000000000 / masterConfig.baudRate;
    masterConfig.lastSckToPcsDelayInNanoSec = 1000000000 / masterConfig.baudRate;
    masterConfig.betweenTransferDelayInNanoSec = 1000000000 / masterConfig.baudRate;

    masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;
    masterConfig.pcsActiveHighOrLow = kLPSPI_PcsActiveLow;

    masterConfig.pinCfg = kLPSPI_SdiInSdoOut;
    masterConfig.dataOutConfig = kLpspiDataOutRetained;

    LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, EXAMPLE_LPSPI_MASTER_CLOCK_FREQ);

    /*Slave config*/
    slaveConfig.bitsPerFrame = masterConfig.bitsPerFrame;
    slaveConfig.cpol = masterConfig.cpol;
    slaveConfig.cpha = masterConfig.cpha;
    slaveConfig.direction = masterConfig.direction;

    slaveConfig.whichPcs = EXAMPLE_LPSPI_SLAVE_PCS_FOR_INIT;
    slaveConfig.pcsActiveHighOrLow = masterConfig.pcsActiveHighOrLow;

    slaveConfig.pinCfg = kLPSPI_SdiInSdoOut;
    slaveConfig.dataOutConfig = kLpspiDataOutRetained;

    LPSPI_SlaveInit(EXAMPLE_LPSPI_SLAVE_BASEADDR, &slaveConfig);

    /******************Set up slave first ******************/
    isSlaveTransferCompleted = false;
    slaveTxCount = 0;
    slaveRxCount = 0;
    whichPcs = EXAMPLE_LPSPI_SLAVE_PCS_FOR_INIT;

    /*The TX and RX FIFO sizes are always the same*/
    g_slaveFifoSize = LPSPI_GetRxFifoSize(EXAMPLE_LPSPI_SLAVE_BASEADDR);

    /*Set the RX and TX watermarks to reduce the ISR times.*/
    if (g_slaveFifoSize > 1)
    {
        txWatermark = 1;
        g_slaveRxWatermark = g_slaveFifoSize - 2;
    }
    else
    {
        txWatermark = 0;
        g_slaveRxWatermark = 0;
    }

    LPSPI_SetFifoWatermarks(EXAMPLE_LPSPI_SLAVE_BASEADDR, txWatermark, g_slaveRxWatermark);

    LPSPI_Enable(EXAMPLE_LPSPI_SLAVE_BASEADDR, false);
    EXAMPLE_LPSPI_SLAVE_BASEADDR->CFGR1 &= (~LPSPI_CFGR1_NOSTALL_MASK);
    LPSPI_Enable(EXAMPLE_LPSPI_SLAVE_BASEADDR, true);

    /*Flush FIFO , clear status , disable all the interrupts.*/
    LPSPI_FlushFifo(EXAMPLE_LPSPI_SLAVE_BASEADDR, true, true);
    LPSPI_ClearStatusFlags(EXAMPLE_LPSPI_SLAVE_BASEADDR, kLPSPI_AllStatusFlag);
    LPSPI_DisableInterrupts(EXAMPLE_LPSPI_SLAVE_BASEADDR, kLPSPI_AllInterruptEnable);

    EXAMPLE_LPSPI_SLAVE_BASEADDR->TCR =
        (EXAMPLE_LPSPI_SLAVE_BASEADDR->TCR &
         ~(LPSPI_TCR_CONT_MASK | LPSPI_TCR_CONTC_MASK | LPSPI_TCR_RXMSK_MASK | LPSPI_TCR_PCS_MASK)) |
        LPSPI_TCR_CONT(0) | LPSPI_TCR_CONTC(0) | LPSPI_TCR_RXMSK(0) | LPSPI_TCR_TXMSK(0) | LPSPI_TCR_PCS(whichPcs);

    /* Enable the NVIC for LPSPI peripheral. Note that below code is useless if the LPSPI interrupt is in INTMUX ,
    * and you should also enable the INTMUX interrupt in your application.
    */
    EnableIRQ(EXAMPLE_LPSPI_SLAVE_IRQN);

    /*TCR is also shared the FIFO , so wait for TCR written.*/
    while (LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_SLAVE_BASEADDR) != 0)
    {
    }
    /*Fill up the TX data in FIFO */
    while (LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_SLAVE_BASEADDR) < g_slaveFifoSize)
    {
        /*Write the word to TX register*/
        LPSPI_WriteData(EXAMPLE_LPSPI_SLAVE_BASEADDR, slaveTxData[slaveTxCount]);
        ++slaveTxCount;

        if (slaveTxCount == TRANSFER_SIZE)
        {
            break;
        }
    }
    LPSPI_EnableInterrupts(EXAMPLE_LPSPI_SLAVE_BASEADDR, kLPSPI_RxInterruptEnable);

    /******************Set up master transfer******************/
    isMasterTransferCompleted = false;
    masterTxCount = 0;
    masterRxCount = 0;
    whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;

    /*The TX and RX FIFO sizes are always the same*/
    g_masterFifoSize = LPSPI_GetRxFifoSize(EXAMPLE_LPSPI_MASTER_BASEADDR);

    /*Set the RX and TX watermarks to reduce the ISR times.*/
    if (g_masterFifoSize > 1)
    {
        txWatermark = 1;
        g_masterRxWatermark = g_masterFifoSize - 2;
    }
    else
    {
        txWatermark = 0;
        g_masterRxWatermark = 0;
    }

    LPSPI_SetFifoWatermarks(EXAMPLE_LPSPI_MASTER_BASEADDR, txWatermark, g_masterRxWatermark);

    LPSPI_Enable(EXAMPLE_LPSPI_MASTER_BASEADDR, false);
    EXAMPLE_LPSPI_MASTER_BASEADDR->CFGR1 &= (~LPSPI_CFGR1_NOSTALL_MASK);
    LPSPI_Enable(EXAMPLE_LPSPI_MASTER_BASEADDR, true);

    /*Flush FIFO , clear status , disable all the inerrupts.*/
    LPSPI_FlushFifo(EXAMPLE_LPSPI_MASTER_BASEADDR, true, true);
    LPSPI_ClearStatusFlags(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_AllStatusFlag);
    LPSPI_DisableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_AllInterruptEnable);

    EXAMPLE_LPSPI_MASTER_BASEADDR->TCR =
        (EXAMPLE_LPSPI_MASTER_BASEADDR->TCR &
         ~(LPSPI_TCR_CONT_MASK | LPSPI_TCR_CONTC_MASK | LPSPI_TCR_RXMSK_MASK | LPSPI_TCR_PCS_MASK)) |
        LPSPI_TCR_CONT(0) | LPSPI_TCR_CONTC(0) | LPSPI_TCR_RXMSK(0) | LPSPI_TCR_TXMSK(0) | LPSPI_TCR_PCS(whichPcs);

    /* Enable the NVIC for LPSPI peripheral. Note that below code is useless if the LPSPI interrupt is in INTMUX ,
    * and you should also enable the INTMUX interupt in your application.
    */
    EnableIRQ(EXAMPLE_LPSPI_MASTER_IRQN);

    /*TCR is also shared the FIFO , so wait for TCR written.*/
    while (LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) != 0)
    {
    }
    /*Fill up the TX data in FIFO */
    while ((LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) < g_masterFifoSize) &&
           (masterTxCount - masterRxCount < g_masterFifoSize))
    {
        /*Write the word to TX register*/
        LPSPI_WriteData(EXAMPLE_LPSPI_MASTER_BASEADDR, masterTxData[masterTxCount]);
        ++masterTxCount;

        if (masterTxCount == TRANSFER_SIZE)
        {
            break;
        }
    }
    LPSPI_EnableInterrupts(EXAMPLE_LPSPI_MASTER_BASEADDR, kLPSPI_RxInterruptEnable);

    /******************Wait for master and slave transfer completed.******************/
    while ((!isSlaveTransferCompleted) || (!isMasterTransferCompleted))
    {
    }

    errorCount = 0;
    for (i = 0; i < TRANSFER_SIZE; i++)
    {
        if (masterTxData[i] != slaveRxData[i])
        {
            errorCount++;
        }

        if (slaveTxData[i] != masterRxData[i])
        {
            errorCount++;
        }
    }
    if (errorCount == 0)
    {
        PRINTF("\r\nLPSPI transfer all data matched! \r\n");
    }
    else
    {
        PRINTF("\r\nError occurred in LPSPI transfer ! \r\n");
    }

    LPSPI_Deinit(EXAMPLE_LPSPI_MASTER_BASEADDR);
    LPSPI_Deinit(EXAMPLE_LPSPI_SLAVE_BASEADDR);

    PRINTF("End of example. \r\n");

    while (1)
    {
    }
}

pin_mux.c

/*
 * Copyright (c) 2016, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 *
 * Redistribution and use in source and binary forms, with or without modification,
 * are permitted provided that the following conditions are met:
 *
 * o Redistributions of source code must retain the above copyright notice, this list
 *   of conditions and the following disclaimer.
 *
 * o Redistributions in binary form must reproduce the above copyright notice, this
 *   list of conditions and the following disclaimer in the documentation and/or
 *   other materials provided with the distribution.
 *
 * o Neither the name of Freescale Semiconductor, Inc. nor the names of its
 *   contributors may be used to endorse or promote products derived from this
 *   software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
 * WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
 * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR
 * ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
 * LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON
 * ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
 * SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */


/*
 * TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: Pins v3.0
processor: MIMXRT1052xxx6A
package_id: MIMXRT1052DVL6A
mcu_data: ksdk2_0
processor_version: 0.0.0
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
 */

#include "fsl_common.h"
#include "fsl_iomuxc.h"
#include "pin_mux.h"

/*
 * TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
BOARD_InitPins:
- options: {callFromInitBoot: 'true', coreID: core0, enableClock: 'true'}
- pin_list:
  - {pin_num: J3, peripheral: LPSPI1, signal: PCS0, pin_signal: GPIO_SD_B0_01, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: J4, peripheral: LPSPI1, signal: SCK, pin_signal: GPIO_SD_B0_00, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: K1, peripheral: LPSPI1, signal: SIN, pin_signal: GPIO_SD_B0_03, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: J1, peripheral: LPSPI1, signal: SOUT, pin_signal: GPIO_SD_B0_02, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: G11, peripheral: LPSPI3, signal: PCS0, pin_signal: GPIO_AD_B0_03, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100,
    drive_strength: R0_6, pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: M14, peripheral: LPSPI3, signal: SCK, pin_signal: GPIO_AD_B0_00, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: M11, peripheral: LPSPI3, signal: SIN, pin_signal: GPIO_AD_B0_02, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: H10, peripheral: LPSPI3, signal: SOUT, pin_signal: GPIO_AD_B0_01, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100,
    drive_strength: R0_6, pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: L14, peripheral: LPUART1, signal: RX, pin_signal: GPIO_AD_B0_13, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
  - {pin_num: K14, peripheral: LPUART1, signal: TX, pin_signal: GPIO_AD_B0_12, slew_rate: Slow, software_input_on: Disable, open_drain: Disable, speed: MHZ_100, drive_strength: R0_6,
    pull_keeper_select: Keeper, pull_keeper_enable: Enable, pull_up_down_config: Pull_Down_100K_Ohm, hysteresis_enable: Disable}
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
 */

/*FUNCTION**********************************************************************
 *
 * Function Name : BOARD_InitPins
 * Description   : Configures pin routing and optionally pin electrical features.
 *
 *END**************************************************************************/
void BOARD_InitPins(void) {
  CLOCK_EnableClock(kCLOCK_Iomuxc);          /* iomuxc clock (iomuxc_clk_enable): 0x03u */

  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_00_LPSPI3_SCK,        /* GPIO_AD_B0_00 is configured as LPSPI3_SCK */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_01_LPSPI3_SDO,        /* GPIO_AD_B0_01 is configured as LPSPI3_SDO */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_02_LPSPI3_SDI,        /* GPIO_AD_B0_02 is configured as LPSPI3_SDI */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_03_LPSPI3_PCS0,       /* GPIO_AD_B0_03 is configured as LPSPI3_PCS0 */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_12_LPUART1_TX,        /* GPIO_AD_B0_12 is configured as LPUART1_TX */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B0_13_LPUART1_RX,        /* GPIO_AD_B0_13 is configured as LPUART1_RX */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_SD_B0_00_LPSPI1_SCK,        /* GPIO_SD_B0_00 is configured as LPSPI1_SCK */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_SD_B0_01_LPSPI1_PCS0,       /* GPIO_SD_B0_01 is configured as LPSPI1_PCS0 */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_SD_B0_02_LPSPI1_SDO,        /* GPIO_SD_B0_02 is configured as LPSPI1_SDO */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinMux(
      IOMUXC_GPIO_SD_B0_03_LPSPI1_SDI,        /* GPIO_SD_B0_03 is configured as LPSPI1_SDI */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_00_LPSPI3_SCK,        /* GPIO_AD_B0_00 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_01_LPSPI3_SDO,        /* GPIO_AD_B0_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_02_LPSPI3_SDI,        /* GPIO_AD_B0_02 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_03_LPSPI3_PCS0,       /* GPIO_AD_B0_03 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_12_LPUART1_TX,        /* GPIO_AD_B0_12 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B0_13_LPUART1_RX,        /* GPIO_AD_B0_13 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_SD_B0_00_LPSPI1_SCK,        /* GPIO_SD_B0_00 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_SD_B0_01_LPSPI1_PCS0,       /* GPIO_SD_B0_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_SD_B0_02_LPSPI1_SDO,        /* GPIO_SD_B0_02 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_SD_B0_03_LPSPI1_SDI,        /* GPIO_SD_B0_03 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */
}

/*******************************************************************************
 * EOF
 ******************************************************************************/

2,977 Views
Yuri
NXP Employee
NXP Employee

Hello,

  CONT (Continuous Transfer) of Transmit Command Register (TCR) should be set with needed

FRAMESZ (say, for several words).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------