LCD backlight Brightness control is not handle using pwm(MIMXRT1064)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD backlight Brightness control is not handle using pwm(MIMXRT1064)

1,271 Views
nikesh
Contributor I

hi all

LCD: rocktech RK043FN66HS
MCU :MIMXRT1064
PWM pin: IOMUXC_GPIO_B1_15_FLEXPWM4_PWMA03

I have taken example code of pwm. In this example code simple led is works perfectly but same way lcd backlight brightness is not works.
I have setup and configure lcd backlight pin as pwm (IOMUXC_GPIO_B1_15_FLEXPWM4_PWMA03), in pwm source code i have change PMW1 to PWM4 and submodule 3.
Any correction in above steps? please let me know.

0 Kudos
Reply
3 Replies

1,228 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nikesh ,

 

Which demo are you referring to ? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,222 Views
nikesh
Contributor I
hi kan_li
I have taken example from driver_examples -> pwm.
PWM1 is use properly same way PWM4 is not work.
please give any suggestion for configuration for PWM4.
0 Kudos
Reply

1,206 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nikesh ,

 

Thanks for the  information! Is it possible to have your code for a review? I will try to reproduce it here.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply