I am using the i.MX RT1176. I can connect via SWD, but I cannot connect via JTAG.
Do I need to configure something in the fuses? Please guide me on how to connect via JTAG.
Thank,
Hi @thanhkaka,
As mentioned on the MIMXRT1170HDUG: "By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use
the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with
other functions"
BR,
Edwin.