Issues when using SDRAM for general data storage on i.MXRT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issues when using SDRAM for general data storage on i.MXRT1176

跳至解决方案
3,997 次查看
JonMcLeanSMC
Contributor II

Hello,

 

I am currently trying to configure the RT1176 to use SDRAM (32MB) for general data/program storage however I am having some issues. Specifically the application stops executing/freezes during the ResetISR function. I have looked at other threads however am yet to find any solution.

 

I have the following predefined symbols:Screen Shot 2022-10-19 at 4.28.02 pm.png

 

I have used the following memory configuration:

 

Screen Shot 2022-10-19 at 4.32.32 pm.png

 

Finally, I provided the following settings for the linker:

Screen Shot 2022-10-19 at 4.34.02 pm.png

 

I am not sure about the heap/stack locations (followed another thread) however even changing those back to default (post data and end respectively) the issue still occurs. Furthermore I am not sure about the Heap being allocated to SDRAM_NCACHE_REGION however another thread suggested that the heap should be allocated to an non cacheable region.

 

Any help would be greatly appreciated. If you need anymore information I'd be happy to provide it

Thanks,
Jon

 

Note: Here is the debug flow when executing the application:

1) Initial Breakpoint at ResetISR

Screen Shot 2022-10-19 at 4.45.10 pm.png

2) First Step Into after initial breakpoint

Screen Shot 2022-10-19 at 4.43.28 pm.png


3) Next Step (throws 0xdeadbeee)

Screen Shot 2022-10-19 at 4.43.52 pm.png

0 项奖励
回复
1 解答
3,908 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @JonMcLeanSMC ,

Add these modification to DCD. It will be fine.

 

Regards,

Jing

在原帖中查看解决方案

7 回复数
3,977 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @JonMcLeanSMC ,

Please use this script file to initialize SDRAM before debug code.

jingpan_0-1666237024095.png

 

Regards,

Jing

3,948 次查看
JonMcLeanSMC
Contributor II

Hi @jingpan ,

Thank you for the response, it proved to be very helpful. I've now set up the script so the SDRAM is initialized before debug however I am still having issues getting my program running.

Instead of failing inside of SystemInit() as before, it will now "fail" upon finishing executing that function (as shown below).

1) Step towards the end of SystemInit() (specifically the SystemInitHook() call)

Screen Shot 2022-10-28 at 2.23.13 pm.png

 

 

 

2) Step Over SystemInitHook()

Screen Shot 2022-10-28 at 2.24.46 pm.png

 

 

 

The memory configuration is still the same as the last post. Any ideas as to what the issue might be? Furthermore I've attached the modified version of your script that I used to initialize the SDRAM (as my board uses JLink/Freelink) in case I have made some stupid mistake.

Thanks,
Jon McLean

0 项奖励
回复
3,940 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @JonMcLeanSMC ,

I made a running in SDRAM demo. It use CMSIS-DAP but jlink should be almost same. Please compare the .ld file.

 

Regards,

Jing

标记 (1)
3,933 次查看
JonMcLeanSMC
Contributor II

Hi @jingpan,

 

I've updated my LD script to more closely match the one you've provided in your example. This has allowed the program to get past the SystemInit function that it was previously failing on. However now it is failing while copying data sections from flash to RAM. When it fails two active faults are shown, specifically BFARVALID(7) and PRECISERR(1). Additionally a FORCED(30) fault is shown.

Here is some screenshots of the fault/registers as well as the debug thread trace:

Screen Shot 2022-11-02 at 12.54.06 pm.png

 

Screen Shot 2022-11-02 at 12.54.12 pm.png

 

I presume the occurence of the faults indicates an issue with the setup of the SEMC however I've gone through and can't find any issues.

Let me know if you have any suggestions.

Thanks,

Jon McLean

Note: I've attached the updated LD script for reference.

0 项奖励
回复
3,923 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @JonMcLeanSMC ,

Is you board a customer board or EVK? If it is your own board, can it pass the SEMC demo in SDK?

 

Regards,

Jing

0 项奖励
回复
3,911 次查看
JonMcLeanSMC
Contributor II

Hi @jingpan ,

It is an third party board (specifically a TQ development kit). After a little bit of modification it does pass the SEMC example. I have modified the SEMC initialization to be the following:

 

    /* Configure SDRAM. */
    sdramconfig.csxPinMux           = kSEMC_MUXCSX0;
    sdramconfig.address             = 0x80000000;
    sdramconfig.memsize_kbytes      = 32 * 1024;       			/* 32MB = 32*1024*1KBytes*/
    sdramconfig.portSize            = kSEMC_PortSize16Bit;		/*two 16-bit SDRAMs make up 32-bit portsize*/
    sdramconfig.burstLen            = kSEMC_Sdram_BurstLen8;
    sdramconfig.columnAddrBitNum    = kSEMC_SdramColunm_9bit;
    sdramconfig.casLatency          = kSEMC_LatencyThree;

    sdramconfig.tPrecharge2Act_Ns   = 18; 						/* tRP 18ns */
    sdramconfig.tAct2ReadWrite_Ns   = 18; 						/* tRCD !(ns */
    sdramconfig.tRefreshRecovery_Ns = 115; 						/* Use the maximum of the (trfc , txsr). */
    sdramconfig.tWriteRecovery_Ns   = 15;  						/* tWR !%ns */
    sdramconfig.tCkeOff_Ns =
        42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/
    sdramconfig.tAct2Prechage_Ns       = 42; 					/* tRAS 40ns */
    sdramconfig.tSelfRefRecovery_Ns    = 115;                   /*Old 70ns;* tXSR*/
    sdramconfig.tRefresh2Refresh_Ns    = 60;                    /*Needs to meet tRFC/tRC timing*/
    sdramconfig.tAct2Act_Ns            = 60; 					/* tRC/tRDD 2ns */
    sdramconfig.tPrescalePeriod_Ns     = 160 * (1000000000 / clockFrq);
    sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */
    sdramconfig.refreshUrgThreshold    = sdramconfig.refreshPeriod_nsPerRow;
    sdramconfig.refreshBurstLen        = 1;
    sdramconfig.delayChain             = 2;

 

 

Thanks,

Jon

0 项奖励
回复
3,909 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @JonMcLeanSMC ,

Add these modification to DCD. It will be fine.

 

Regards,

Jing