Issue in Flashing the Hex file using NXP boot utility V3.5.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue in Flashing the Hex file using NXP boot utility V3.5.0

1,458 次查看
S_Rai
Contributor I

Hello,

We are trying to flash the Hex file generated into our board which has MIMXRT1176DVMAA controller using NXP boot utility tool.

Its giving an error as FlexSPI write alignment error.

But the bin file of the same application can be loaded and is working fine.

What might be the issue?

Regards

Sanath

0 项奖励
回复
3 回复数

1,441 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @S_Rai ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I was wondering if you can share the log of the NXP boot utility V3.5.0, further, please illustrates the steps of generating the hex file.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,435 次查看
S_Rai
Contributor I

Hi jeremyzhou,

 

Thank you for the reply.

1. Below is the Log from NXP boot utility.

S_Rai_0-1667365692084.png

.

2.I am converting the .axf file to .hex file from MCU Xpresso Binary Utilities option .

the .bin file which is being converted in same way is working when we dump using NXP boot utility.

S_Rai_1-1667365844419.png

Regards

Sanath

0 项奖励
回复

1,429 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @S_Rai ,
Thanks for your reply.
Actually, you need to adjust the linker file and modify related macros prior to generating the axf, so please refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复