Hello NXP,
To reduce the size of my custom board as per the requirement, I want use the flash memory as ram in order to meet the ram requirement of the applications that includes the camera and LCD which requires large data buffers. So I want to know the following.
Q1. Is there any way to convert and use the external flash present on the board as ram ?
Q2. If so can you provide me the base example code ?. Which will be helpful.
Q3.Else are there any other ways to run the camera streaming and LCD applications without the external SDRAM?
Thanks in advance for the help.
Regards,
Ragnar.