We are looking to use MQS to generate some tones in our system directly from a const array in flash.
Can I get permission on this link?
About the example code of MQS, It runs on RT1050 EVB, and is based on SDK_2.3.0_EVK-MIMXRT1050. To build and run the demo, extract the archive file into the directory SDK_2.3.0_EVK-MIMXRT1050\boards\evkmimxrt1050\user_apps. And replace the driver file SDK_2.3.0_EVK-MIMXRT1050\devices\MIMXRT1052\drivers\fsl_sai_edma.c with the attached one to fix a bug. About the example code you can get them here https://community.nxp.com/message/1005849.
Hi Rita,
I am not allowed to the what is in the link.. not sure if it is a me thing or a community thing. Does the example you provide allow the creation of the tones or just pipe an input to an output?
thanks again,
John