Is i.MX RT device support “Plain load image”

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is i.MX RT device support “Plain load image”

1,117 Views
zhoup
Contributor I

Now I use rt1064 for developing,i want my applilcation programmed into internal flash(4MB), but boot rom will relocatie it into OC_RAM。

I think “Plain load image” is just i want, but it is only support LPC54xx untill now?

zhoup_3-1651125617355.png

 

i have try use SDK example "freertos_hello" for testing, unfortunately,it does not run properly。

0 Kudos
Reply
1 Reply

1,111 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it's a typical non-XIP mode, you can learn it via the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply