Interface with Alexa (568-SLN-ALEXA-IOT-ND )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface with Alexa (568-SLN-ALEXA-IOT-ND )

799 Views
a_k_alhazmi
Contributor I

Hi,

I am working on project that collecting data form the sensor and plotted them by Matlab. I want to interface my system with Alexa, so when my sensor detect the level is low then Alexa will speak up " Are you good " without being prompted.

So, is there any way that allowed to program Alexa to receive the data from my sensor and let her speak up without being prompted as per my requirement. 

Labels (1)
0 Kudos
Reply
1 Reply

740 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I believe this is possible, however we do not have at the moment support/guides to describe how this can be done. I'd highly recommend to check Amazon's documentation. There are some skills that allow you to get notifications such as in the following link.

Notifications Overview | Alexa Voice Service 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply