Inquiry About Porting Matter Thermostat to RT1060 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry About Porting Matter Thermostat to RT1060 EVK

Jump to solution
635 Views
pooisonner
Contributor III

 

Hello, I am currently implementing a Matter thermostat using the RT1060 EVK.
I have been setting up the development environment for a few weeks.
My development environment is Windows 11 with VirtualBox installed, running Ubuntu 22.04.
After that, I set up the development environment with VS Code and have successfully built the thermostat example.
However, I am unsure about how to port it to the board.
The EVK board has an LPC4322 with OpenSDA as the default.
Downloading via the debug button in VS Code does not work.
I would like to ask how I should proceed.
Thank you.

0 Kudos
Reply
1 Solution
515 Views
Sam_Gao
NXP Employee
NXP Employee

Hi, 

I suggest you use the native method (EVK board connected to Windows or Ubuntu on PC). I don't recommend this method you mentioned because I can't be sure if there is a problem between Ubuntu-VM-Windows.

View solution in original post

0 Kudos
Reply
5 Replies
614 Views
Sam_Gao
NXP Employee
NXP Employee

@pooisonner 

You built the SDK on the ubuntu which was installed in VirtualBox running on the Windows, the hardware rt1060-evk is connected to the Windows, you want to flash the firmware into the evk board from the ubuntu, is it correct for my understanding?

 

0 Kudos
Reply
534 Views
pooisonner
Contributor III

Hello,
I am awaiting a response regarding my previous inquiry.
I am experiencing difficulties in development due to the download not working.
Please provide a reply.
Thank you.

0 Kudos
Reply
534 Views
pooisonner
Contributor III
Hello,
I am awaiting a response regarding my previous inquiry.
I am experiencing difficulties in development due to the download not working.
Please provide a reply.
Thank you.
0 Kudos
Reply
597 Views
pooisonner
Contributor III

Yes, that's correct.

In Ubuntu on VirtualBox, the EVK board can be recognized by mounting it via USB, and CMSIS-DAP is recognized in VSCode.

However, I'm contacting you because the download does not proceed afterward.

Thank you.

0 Kudos
Reply
516 Views
Sam_Gao
NXP Employee
NXP Employee

Hi, 

I suggest you use the native method (EVK board connected to Windows or Ubuntu on PC). I don't recommend this method you mentioned because I can't be sure if there is a problem between Ubuntu-VM-Windows.

0 Kudos
Reply