解決済! 解決策の投稿を見る。
The problem has been resolved, the HIFI4 needs to register the activation interrupt mechanism.
The problem has been resolved, the HIFI4 needs to register the activation interrupt mechanism.
Hi @Padi-2023 ,
Hope you are doing well!
Could you help me check this AN: 8-channel DMIC Audio Acquisition on RT600 HiFi4 (nxp.com)
There are two DMA controllers in i.MX RT600. Generally, the main recommended usage method is to allocate DMA0 to CM33 and DMA1 to HiFi4. There are several points to note when using DMA in HiFi4:
• HiFi4 interrupt should be registered and enabled in XOS or XTOS. The XOS is an embedded kernel from Cadence is designed for efficient operation on embedded systems built and the XTOS is a single-threaded runtime for Xtensa processors.
• The SRAM address of DMA operation needs to be non-cacheable.
• HiFi4 interrupt needs to be configured by INPUTMUX
Best regards,
Gavin