hello supporter, In My Customized imrt1176 board ,we use the ENET_QOS MAC to connect a KSZ8081 PHY, with "enet_qos_txrx_mulitring sdk example " ,we can get the phy id from the mdio interface ,we can
auto negoiate from the remote 100M port ,but we failed at DMA reset ,following is the Schematic , please help to review it .
Hello @wangdabing .
From the schematic and I can't find the obvious issue and you may check the config of the development board as the below:
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------